2023-03-26 09:21 PM
2023-03-26 09:27 PM
These are the pinout and clock config diagram
I am working with STM32F407 to write a text file to Pen drive (USB Host).
f_open(&MyFile, "testfile.txt", FA_CREATE_ALWAYS | FA_WRITE);
getting FD_DISC_ERR. When I debugged more i understood that this is due to HOST_DEV_WAIT_FOR_ATTACHMENT issue. Can anyone help why this is happening?
2023-03-28 04:07 AM
Hello @Ajithkumar and welcome to the Community
Try ClockDiv with 2 or 4.
I advise you to get inspired from the available examples available with STM32CubeF4 MCU package, and you will find more details on this article: Introduction to USB with STM32.
Make sure to use latest versions of STM32CubeMX and STM32CubeF4 MCU package.
Imen
2023-03-30 09:50 PM
Not worked. I tried with multiple clock vales.
I tried with example project in CudeIDE as well as i created new project from scratch but not worked me both.
Is any Size limitation for Flash Drive size ?
I mean I tried with 16GB and 32GB Flash Drive