cancel
Showing results for 
Search instead for 
Did you mean: 

I am using X-CUBE-AWS packages with p-l496g-cell01 development board to send my sensor data on AWS it works fine buy during sometime code will stick and it generates an error

pragnesh
Associate III

I am using X-CUBE-AWS packages with p-l496g-cell01 development board to send my sensor data on AWS it works fine buy during sometime code will stick and it generates an error

I also enable "isAutoReconnectEnabled" flag but it genrate error like

ERROR: ../../../../../../Middlewares/ST/STM32_Connect_Library/services/net_mbedtls.c:367 failed

 ! mbedtls_ssl_read returned -0x7880

ERROR: iot_tls_read L#209 net_recv failed - -109

2000aaf8 => ../../../../../../Middlewares/Third_Party/mbedTLS/library/ssl_tls.c:6940: => read

2000aaf8 => ../../../../../../Middlewares/Third_Party/mbedTLS/library/ssl_tls.c:3809: => read record

2000aaf8 => ../../../../../../Middlewares/Third_Party/mbedTLS/library/ssl_tls.c:2252: => fetch input

2000aaf8 => ../../../../../../Middlewares/Third_Party/mbedTLS/library/ssl_tls.c:2412: in_left: 0, nb_want: 5

com_recv in progress of 5 bytes

2000aaf8 => ../../../../../../Middlewares/Third_Party/mbedTLS/library/ssl_tls.c:2436: in_left: 0, nb_want: 5

2000aaf8 => ../../../../../../Middlewares/Third_Party/mbedTLS/library/ssl_tls.c:7330: => write

2000aaf8 => ../../../../../../Middlewares/Third_Party/mbedTLS/library/ssl_tls.c:2764: => write record

2000aaf8 => ../../../../../../Middlewares/Third_Party/mbedTLS/library/ssl_tls.c:1287: => encrypt buf

2000aaf8 => ../../../../../../Middlewares/Third_Party/mbedTLS/library/ssl_tls.c:1443: before encrypt: msglen = 10, including 0 bytes of padding

2000aaf8 => ../../../../../../Middlewares/Third_Party/mbedTLS/library/ssl_tls.c:1605: <= encrypt buf

2000aaf8 => ../../../../../../Middlewares/Third_Party/mbedTLS/library/ssl_tls.c:2907: output record: msgtype = 23, version = [3:3], msglen = 26

2000aaf8 => ../../../../../../Middlewares/Third_Party/mbedTLS/library/ssl_tls.c:2471: => flush output

2000aaf8 => ../../../../../../Middlewares/Third_Party/mbedTLS/library/ssl_tls.c:2489: message length: 31, out_left: 31

Trying to send (31) on socket 0

ERROR: ../../../../../../Middlewares/ST/STM32_Connect_Library/netif/cellular_if/net_cellular.c:671 Send failed : 4294967290

ERROR: ../../../../../../Middlewares/ST/STM32_Connect_Library/services/net_mbedtls.c:490 mbedtls_net_send(): error -21 in send() - requestedLen=31

2000aaf8 => ../../../../../../Middlewares/Third_Party/mbedTLS/library/ssl_tls.c:2496: ssl->f_send() returned -30848 (-0x7880)

2000aaf8 => ../../../../../../Middlewares/Third_Party/mbedTLS/library/ssl_tls.c:2918: mbedtls_ssl_flush_output() returned -30848 (-0x7880)

2000aaf8 => ../../../../../../Middlewares/Third_Party/mbedTLS/library/ssl_tls.c:7277: mbedtls_ssl_write_record() returned -30848 (-0x7880)

2000aaf8 => ../../../../../../Middlewares/Third_Party/mbedTLS/library/ssl_tls.c:7358: <= write

ERROR: ../../../../../../Middlewares/ST/STM32_Connect_Library/services/net_mbedtls.c:387 failed

 ! mbedtls_ssl_write returned -0x7880

ERROR: iot_tls_write L#165 failed

 ! mbedtls_ssl_write returned -0x6d

2000aaf8 => ../../../../../../Middlewares/Third_Party/mbedTLS/library/ssl_tls.c:7373: => write close notify

2000aaf8 => ../../../../../../Middlewares/Third_Party/mbedTLS/library/ssl_tls.c:2471: => flush output

2000aaf8 => ../../../../../../Middlewares/Third_Party/mbedTLS/library/ssl_tls.c:2489: message length: 31, out_left: 31

Trying to send (31) on socket 0

ERROR: ../../../../../../Middlewares/ST/STM32_Connect_Library/netif/cellular_if/net_cellular.c:671 Send failed : 4294967290

ERROR: ../../../../../../Middlewares/ST/STM32_Connect_Library/services/net_mbedtls.c:490 mbedtls_net_send(): error -21 in send() - requestedLen=31

2000aaf8 => ../../../../../../Middlewares/Third_Party/mbedTLS/library/ssl_tls.c:2496: ssl->f_send() returned -30848 (-0x7880)

2000aaf8 => ../../../../../../Middlewares/Third_Party/mbedTLS/library/ssl_tls.c:7542: => free

2000aaf8 => ../../../../../../Middlewares/Third_Party/mbedTLS/library/ssl_tls.c:7607: <= free

Trying to close socket 0

socket 0 is now closed

WARN: disconnectCallbackHandler L#149 MQTT Disconnect

Auto Reconnect is enabled, Reconnecting attempt will start now

In short my reconnection is not working and code will be stuck 

Any one idea about this

This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
JGENT
Associate II

​Hello,

The message 0x7880  is described here : https://tls.mbed.org/api/ssl_8h.html . It means that “The peer notified us that the connection is going to be closed�? . But in fact this message is the one returned by the socket wrapperbelow MbedTLS , see file “net_mbedtls.c�? , at that stage the wrapper miss information to make the distinction between the different error case.

     MBEDTLS_ERR_SSL_INTERNAL_ERROR,

     MBEDTLS_ERR_SSL_PEER_CLOSE_NOTIFY,

     MBEDTLS_ERR_SSL_CONN_EOF.

 So in case of error , the wrapper always return the  "MBEDTLS_ERR_SSL_PEER_CLOSE_NOTIFY" error.  This happen  while performing a write to a socket, see functionbelow.

The error is coming the lower part of the stack  ,the Cellular driver is the one which returns this error.  So shoul add Cellular tag to this  issue to see if cellular competent people can help.

 Br,

 Jean-Marc

static int32_t mbedtls_net_send(void *ctx, const uchar_t *buf, size_t len)

 if (pSocket->write_timeout == 0)

 {

   flags = (int8_t) NET_MSG_DONTWAIT;

 }

 UNLOCK_SOCK(pSocket->idx);

 /*cstat -MISRAC2012-Rule-11.8 removing const attribute */

 ret = pSocket->pnetif->pdrv->psend(pSocket->ulsocket, (uchar_t *) buf, len, flags);

 /*cstat +MISRAC2012-Rule-11.8 */

 LOCK_SOCK(pSocket->idx);

 if (ret >= 0)

 {

   if (ret == 0)

   {

     ret = MBEDTLS_ERR_SSL_WANT_WRITE;

   }

 }

 else

 {

   NET_DBG_ERROR("mbedtls_net_send(): error %ld in send() - requestedLen=%d\n", ret, len);

   /* TODO: The underlying layers do not allow to distinguish between

   *         MBEDTLS_ERR_SSL_INTERNAL_ERROR,

   *         MBEDTLS_ERR_SSL_PEER_CLOSE_NOTIFY,

   *         MBEDTLS_ERR_SSL_CONN_EOF.

   * Most often, the error is due to the closure of the connection by the remote host. */

   ret = MBEDTLS_ERR_SSL_PEER_CLOSE_NOTIFY;

}