2022-08-16 3:54 PM
I will mention at this point that I am connecting to a known working CDC device. I know it is working because I can connect the same port to a PC, and it enumerates properly, and I can pass data to/from the device.
In module usbh_core.c function USBH_Process() the state HOST_ENUMERATION gets set but fails to complete. That is, the call to 'status = USBH_HandleEnum(phost);' never returns USBH_OK so the process times out and the state gets set back to HOST_IDLE.
Has anyone seen this problem before?
2022-08-26 7:11 AM
Hello @BBert ,
You can refer to the following example provided under the F4 Firmware Package:
I hope this helps.
BeST Regards,
Walid