cancel
Showing results for 
Search instead for 
Did you mean: 

How to use transfer learning to perform image classification on STM32

beijing
Associate

How should a new STM32H747I-DISCO be used, why does the display not start after I connect the computer with st-link and display 32kb of memory

This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
Dor_RH
ST Employee

Hello @beijing,

To prevent ST-Link connection problems, confirm that your development environment is configured for the appropriate target device. Additionally, regularly update the embedded firmware to access new features or corrections. Detailed information is available in the ST-LINK derivatives technical note (TN1235) on st.com.

For proper booting, verify the boot jumpers on the board are set correctly to boot from the designated memory. For detailed guidance on configuring and resolving issues with the display, refer to the STM32H747I-DISCO user manual (UM2411) on st.com.

Thanks and Best Regards,

Dorsaf