cancel
Showing results for 
Search instead for 
Did you mean: 

How to use HAL_PCDEx_SetTxFiFo on STM32F4 when porting from STM32F0

Nix Wayne
Associate III

Hi,

I am migrating some USB code which was initially developed on STM32F0.

There are 6 end points in use (including control):

EP address:

0x0

0x80

0x87 -

0x81

0x01

0x82

So my code to config PMA in USB_LL_Init:

HAL_PCDEx_PMAConfig((PCD_HandleTypeDef*)pdev->pData , 0x00 , PCD_SNG_BUF, 0x18);
HAL_PCDEx_PMAConfig((PCD_HandleTypeDef*)pdev->pData , 0x80 , PCD_SNG_BUF, 0x58);
HAL_PCDEx_PMAConfig((PCD_HandleTypeDef*)pdev->pData , 0x87, PCD_SNG_BUF, 0x98);  
HAL_PCDEx_PMAConfig((PCD_HandleTypeDef*)pdev->pData , 0x81, PCD_SNG_BUF, 0xD8);  
HAL_PCDEx_PMAConfig((PCD_HandleTypeDef*)pdev->pData , 0x01, PCD_SNG_BUF, 0x13C); 	
HAL_PCDEx_PMAConfig((PCD_HandleTypeDef*)pdev->pData , 0x82, PCD_SNG_BUF, 0x1A0);  

and this works fine on STM32F0.

Now I am migrating this same code to STM32F4 and here is a bit different. Using HAL_PCDEx_SetRxFiFo and HAL_PCDEx_SetTxFifo. As below:

HAL_PCDEx_SetRxFiFo(&hpcd_USB_FS, 0x40);
HAL_PCDEx_SetTxFiFo(&hpcd_USB_FS, 0, 0x40); // EP0

So my understanding is that my old code translates into something like this:

HAL_PCDEx_SetRxFiFo(&hpcd_USB_FS, 0x40); // 0x0
HAL_PCDEx_SetTxFiFo(&hpcd_USB_FS, 0, 0x40); // 0x80
HAL_PCDEx_SetTxFiFo(&hpcd_USB_FS, 7, 0x40); // 0x87
HAL_PCDEx_SetTxFiFo(&hpcd_USB_FS, 1, 0x40); // 0x81
HAL_PCDEx_SetTxFiFo(&hpcd_USB_FS, 2, 0x40); // 0x82
	

Is this correct or am I missing something?

This discussion is locked. Please start a new topic to ask your question.
6 REPLIES 6
waclawek.jan
Super User

I don't use Cube/HAL, but these functions might expect size in words, and might be expected to be called in a rigorous order, i.e. Rx first, then Tx in their natural order.

You also need the common Rx buffer be big enough to accomodate the biggest Out packet (plus some overhead).

JW

Nix Wayne
Associate III

I made general mistake. Number coresponds to pipe address. F4 ha 5In/OUT EP. RX fifo is common and TX can be assigned to each EP.

So digging into CMSIS drivers they predefine FIFO's with constant values.

Dividing 1.25k by two. One half is RX fifo and other half divides to another 5 for each TX EP.

So a call shoud be

HAL_PCDEx_SetTxFiFo(&hpcd_USB_FS, x, 0x40); where x goes from 0 to 5.

and coresponds to addresses 0x80...0x85

What I did in my project is switch of EP 0x87 to 0x83 and it works fine.

hakan23
Associate II

Hello Nix

I'm in the same situation porting code but from STM32F4 to STM32F7.

Can you please clearify how it works ??

I have

 HAL_PCDEx_PMAConfig(pdev->pData , RNDIS_CONTROL_OUT_EP    , PCD_SNG_BUF, RNDIS_CONTROL_OUT_PMAADDRESS);

 HAL_PCDEx_PMAConfig(pdev->pData , RNDIS_CONTROL_IN_EP     , PCD_SNG_BUF, RNDIS_CONTROL_IN_PMAADDRESS);

 HAL_PCDEx_PMAConfig(pdev->pData , RNDIS_NOTIFICATION_IN_EP  , PCD_SNG_BUF, RNDIS_NOTIFICATION_IN_PMAADDRESS);  

 HAL_PCDEx_PMAConfig(pdev->pData , RNDIS_DATA_OUT_EP      , PCD_SNG_BUF, RNDIS_DATA_OUT_PMAADDRESS);

 HAL_PCDEx_PMAConfig(pdev->pData , RNDIS_DATA_IN_EP      , PCD_SNG_BUF, RNDIS_DATA_IN_PMAADDRESS);  

where

define RNDIS_CONTROL_OUT_EP              0x00

#define RNDIS_CONTROL_IN_EP               0x80

#define RNDIS_NOTIFICATION_IN_EP            0x81

#define RNDIS_DATA_IN_EP                0x82

#define RNDIS_DATA_OUT_EP                0x03

and

#define RNDIS_CONTROL_OUT_PMAADDRESS          0x08 * 4        //8 bytes per EP

#define RNDIS_CONTROL_IN_PMAADDRESS           RNDIS_CONTROL_OUT_PMAADDRESS + USB_MAX_EP0_SIZE

#define RNDIS_NOTIFICATION_IN_PMAADDRESS        RNDIS_CONTROL_IN_PMAADDRESS + USB_MAX_EP0_SIZE

#define RNDIS_DATA_IN_PMAADDRESS            RNDIS_NOTIFICATION_IN_PMAADDRESS + RNDIS_NOTIFICATION_IN_SZ

#define RNDIS_DATA_OUT_PMAADDRESS            RNDIS_DATA_IN_PMAADDRESS + RNDIS_DATA_IN_SZ

How will this translate into

HAL_PCDEx_SetRxFiFo and HAL_PCDEx_SetTxFiFo calls ??

Thanks in advance

waclawek.jan
Super User

> from STM32F4

Which 'F4?

The Device-only USB generally sets FIFOs as byte-addresses, while the FIFO settings in the OTG_USB are in 32-bit words.

Read the comments I wrote above. I don't use Cube/HAL.

JW

hakan23
Associate II

​I'm trying to port

https://github.com/fetisov/lrndis

to a STM32F746G-Discovery board

I will look in to your answer more deeply

Thanks

ALin.6
Associate II

As above configure, only display "Serial Port Com", can not display "RNDIS ethernet" ? So what is the problem?