2019-02-21 1:24 AM
2019-02-21 3:16 AM
Connect the FTDI UART to the bootloader UART. Eventuallly connect BOOT 0 to the FTDI to switch to UART bootloader mode. Use the STM tools or stm32flash. If the FTDI has MPSSE, you could do a variant of the Bl*ck M*gic debug probe with the libftdi platform https://github.com/blacksphere
2019-02-21 3:09 PM
Thanks Uwe, all looks too hard, I'm gonna get me a ST-Link V2 and use the ST-Link software. I was just trying to solve a problem on the spot, but now I'll just wait until the ST-Link V2 arrives. :)
2019-02-21 5:34 PM
The device can be programmed via USART1 PA9/PA10, reset the device with BOOT0 High, and it will enter the ROM based System Loader. Use STM32 Cube Programmer to connect to a COM port, from a FTDI USB-to-Serial adapter.
2019-02-24 7:36 PM
Thanks Clive. I made up an adaptor for my FTDI to connect to my board, but it turns out I have a problem on my board preventing it going into DFU mode. I'm looking into that now.