2026-05-07 7:09 AM - last edited on 2026-05-07 7:10 AM by mƎALLEm
Hi Technical Support Team,
I am working with the Nucleo-H563ZI board and would like to enable the I3C interface within the Zephyr environment.
Could you provide a minimal sample project or a reference configuration (Devicetree/Kconfig) to validate the I3C host driver and I3C shell?
Thank you for your assistance.
----------------------------------------------
prj.conf
CONFIG_I3C=y
CONFIG_I3C_SHELL=y
CONFIG_I3C_STM32=y
CONFIG_USERSPACE=y
CONFIG_I3C_RTIO=y
----------------------------------------------
Solved! Go to Solution.
2026-05-12 4:14 PM
Hi Hamdi,
The minimal configuration works well.
Thank you for your support
Alvin
2026-05-07 8:42 AM
Hello @Alvin0916
Please refer to the following video:
Using I3C bus for connecting I3C and I2C sensors - Zephyr Meetup Prague
2026-05-07 12:47 PM - edited 2026-05-07 1:31 PM
Hi Saket_Om,
Could you let me know which Zephyr version this demo is implemented with?
compiler environment # Zephyr version :4.3.99
Is the arduino_i3c: &i3c1 {}; line necessary for the I3C driver to work?
Would it be possible for you to review the nucleo_h563zi.overlay?
#video's Timestamp at 10:53
------------------------nucleo_h563zi.overlay-------------------------
&i3c1 {
pinctrl-0 = <&i3c1_scl_pd12 &i3c1_sda_pd13>;
pinctrl-names = "default";
status = "okay";
clocks = <&rcc STM32_CLOCK(APB1, 23U)>,
<&rcc STM32_SRC_HSI I3C1_SEL(2)>;
i2c-scl-hz = <400000>;
i3c-scl-hz = <6000000>;
}
-------------------------------------------ref info-----------------------------
/* /home/alvin/zephyrproject/zephyr/boards/st/nucleo_h563zi/nucleo_h563zi-common.dtsi */
&i3c1 {
pinctrl-0 = <&i3c1_scl_pd12 &i3c1_sda_pd13>;
pinctrl-names = "default";
i3c-scl-hz = <12500000>;
status = "okay";
};
&rcc {
clocks = <&pll>;
clock-frequency = <DT_FREQ_M(240)>;
ahb-prescaler = <1>;
apb1-prescaler = <2>;
apb2-prescaler = <1>;
apb3-prescaler = <2>;
};
/* /home/alvin/zephyrproject/zephyr/dts/arm/st/h5/stm32h5.dtsi */
i3c1: i3c@40005c00 {
compatible = "st,stm32-i3c";
reg = <0x40005c00 0x400>;
interrupts = <123 0>, <124 0>;
interrupt-names = "event", "error";
#address-cells = <3>;
#size-cells = <0>;
clocks = <&rcc STM32_CLOCK(APB1, 23)>;
resets = <&rctl STM32_RESET(APB1L, 23)>;
zephyr,pm-device-runtime-auto;
status = "disabled";
};
rcc: rcc@44020c00 {
compatible = "st,stm32h5-rcc";
clocks-controller;
#clock-cells = <2>;
reg = <0x44020c00 0x400>;
rctl: reset-controller {
compatible = "st,stm32-rcc-rctl";
#reset-cells = <1>;
};
};
2026-05-08 7:26 AM - edited 2026-05-08 7:37 AM
Hello @Alvin0916
Yes —arduino_i3c: &i3c1 {}; is not necessary for the I3C driver to work.
For your overlay, the simple recommended version is:
&i3c1 {
i2c-scl-hz = <400000>;
i3c-scl-hz = <6000000>;
};
&i3c1 is already enabled in nucleo_h563zi-common.dtsi, so you do not need to repeat the following:
pinctrl-0 = <&i3c1_scl_pd12 &i3c1_sda_pd13>;
pinctrl-names = "default";
status = "okay";
I also suggest removing the clocks line for now, unless you have a confirmed reason to override it.
with regrads,
Hamdi
2026-05-12 4:14 PM
Hi Hamdi,
The minimal configuration works well.
Thank you for your support
Alvin