cancel
Showing results for 
Search instead for 
Did you mean: 

How to display the uart data on stm32f429i eval board?

PSR1
Associate III

Hello ST,

 I'm trying  to display the uart data on stm32f429i(MB1046) eval board GUI, followed below link as 

https://controllerstech.com/touchgfx-5-data-from-uart-to-ui/,

 
void HAL_UARTEx_RxEventCallback(UART_HandleTypeDef *huart, uint16_t Size)

{

RxData[Size] = '\0';

if (osMessageQueueGetSpace(uartQueueHandle)>0)

{

strncpy (uartData_q->Data, (char *)RxData, Size+1);

uartData_q->size = Size+1;

osMessageQueuePut(uartQueueHandle, &uartData_q, 0, 0);

HAL_UART_Transmit(&huart1, uartData_q->Data,uartData_q->size , 1000);

}

HAL_UARTEx_ReceiveToIdle_IT(&huart1, RxData, 256);

}

void StartDefaultTask(void *argument)

{

/* USER CODE BEGIN 5 */

HAL_UARTEx_ReceiveToIdle_IT(&huart1, RxData, 256);



/* Infinite loop */

for(;;)

{

osDelay(1000);

}

/* USER CODE END 5 */

}

This code added in main.c but uart  receive interrupt is not working.

could you please help me to develop.


Thanks& Regards,

PSR.

15 REPLIES 15

yes,

Right: and you've demonstrated that both UART1 and UART7 work together without FreeRTOS 7 TouchGFX?

So this code works in a standalone project:

   HAL_UART_Transmit(&huart1, TxData, 256 , 1000);

   HAL_UART_Receive (&huart7, RxData, strlen((char *)TxData), HAL_MAX_DELAY);
   HAL_UART_Transmit(&huart7, RxData, strlen((char *)RxData), 100);

?

A complex system that works is invariably found to have evolved from a simple system that worked.
A complex system designed from scratch never works and cannot be patched up to make it work.

yes, this transmission working fine.

Could you please go through the attached https://controllerstech.com/touchgfx-5-data-from-uart-to-ui/ , based on this i was generated the code  and added the code. after you will get idea about task. please go through.

Thanks,

PSR

PSR1
Associate III

Hello, Andrew Neil.

Is there any update?

Thanks &Regards,

PSR.

So what debugging have you done on your FreeRTOS version?

Compare & contrast against the standalone version - see where they differ.

A complex system that works is invariably found to have evolved from a simple system that worked.
A complex system designed from scratch never works and cannot be patched up to make it work.

@PSR1 wrote:

I have quick test on attached code, please go through,
could you please me to develop uart data on stm32f429 i eval display?

Thanks ,

PSR

 

 

void StartDefaultTask(void *argument)
{
  /* USER CODE BEGIN 5 */
	   HAL_UART_Transmit(&huart1, TxData, 256 , 1000);

	   HAL_UART_Receive(&huart7, RxData, strlen((char *)TxData), HAL_MAX_DELAY);
          HAL_UART_Transmit(&huart7, RxData, strlen((char *)RxData), 100);
  /* Infinite loop */
  for(;;)
  {
    osDelay(1000);
  }
  /* USER CODE END 5 */
}

 

 


Not sure why FreeRTOS would have anything to do with UART7 not working, given the code is before the for loop?

The only thing I can think of is if your RxData doesn't start with characters, then the strlen will return 0. Calling HAL_UART_Transmit would not send any data

So are you sure RxData has a string and doesn't start with a null?

If a reply has proven helpful, click on Accept as Solution so that it'll show at top of the post.
CAN Jammer an open source CAN bus hacking tool
CANableV3 Open Source