2019-02-03 10:17 PM
I am looking for a way to change the HAL I2C lib clock speed during runtime to either 100k or 400k or 1M.
I tried the following.....
hi2c1.Init.ClockSpeed = 100000;
However when compiling this the compiler do not recognize the parameter.
Solved! Go to Solution.
2019-02-05 3:28 AM
Hi @fglau ,
The I2C speed configuration is based on I2C_TIMINGR register content.
So, in the HAL structure, you need to program properly the parameter hi2c1.Init.Timing:
hi2c1.Init.Timing = I2C_TIMING;
I2C_TIMING value depends on:
The appropriate value may be calculated using STM32CubeMX interface: you will see that a suitable value for TIMINGR will be suggested depending on what you provide as inputs.
-Amel
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2019-02-03 10:18 PM
I forgot to mention - this is for the STM32H7 HAL I2C lib
2019-02-04 1:17 AM
You'd need to reintialize with the new values in the structure or disable the peripheral, change the clock parameters, and then enable again.
2019-02-04 1:53 AM
Yes changing the speed and then calling MX_I2C1_Init(); again make sense - however
I cannot find the register for the STM32H7xx in the HAL I2C lib to set the new SCL clock rate.
I tried hi2c1.Init.ClockSpeed = 100000; but the Atollic compiler did not recognize the HAL parameter
Which parameter should i change to update the speed??
2019-02-05 3:28 AM
Hi @fglau ,
The I2C speed configuration is based on I2C_TIMINGR register content.
So, in the HAL structure, you need to program properly the parameter hi2c1.Init.Timing:
hi2c1.Init.Timing = I2C_TIMING;
I2C_TIMING value depends on:
The appropriate value may be calculated using STM32CubeMX interface: you will see that a suitable value for TIMINGR will be suggested depending on what you provide as inputs.
-Amel
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2019-02-05 4:21 PM
OK thanks Amel that worked just fine.
2021-06-30 7:36 AM
Hello @Amel NASRI
where can I find the formula used by CubeMx to calculate I2C_TIMING?
Thanks.
2021-07-01 2:15 AM
Hello @RDums.1 ,
I2C_TIMING calculation in STM32CubeMX is based on formulas described in the RM. You need to refer to I2C timing register (I2C_TIMINGR).
For any follow-up question, please submit a new discussion as the current one is old.
-Amel
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.