cancel
Showing results for 
Search instead for 
Did you mean: 

How to change baud rate of serial port uart in runtime stm32f4?

sonminh
Associate II

 

Hi everybody,

I use UART6 of STM32F437 and want to change baud rate between baud rate 115200, 460800 and 921600 in runtime

I've followed some answers from a post here:

https://stackoverflow.com/questions/57283327/how-to-change-the-uart-baud-rate-after-running-on-stm32-board

USART6 -> CR1 &= ~(USART_CR1_UE);

USART6 -> BRR = NEWVALUE;

USART6 -> CR1 |= USART_CR1_UE;

But still can't seem to get the baud rate to change. Has anyone change the baud rate of the UART successful?

/****************************************************/

Thanks and brgs 

5 REPLIES 5
Andrew Neil
Super User

Have you checked the Datasheet and/or Reference Manual ?

https://www.st.com/en/microcontrollers-microprocessors/stm32f437ai.html#documentation

(Product Page doesn't seem to be working for me at the moment)

A complex system that works is invariably found to have evolved from a simple system that worked.
A complex system designed from scratch never works and cannot be patched up to make it work.

Rather than just UE, does it help if you (also) clear TE and/or RE for the change?

 

A complex system that works is invariably found to have evolved from a simple system that worked.
A complex system designed from scratch never works and cannot be patched up to make it work.

Thanks for your reply

 

Can you talk clearly? Do you have sample code to change baud rate uart runtime

Sorry, no. It was just a suggestion - something for you to try.

A complex system that works is invariably found to have evolved from a simple system that worked.
A complex system designed from scratch never works and cannot be patched up to make it work.
LCE
Principal II

As @Andrew Neil said, try to disable TE & RE in CR1 before changing baud rate.

From RM0090:

30.6.3 Baud rate register (USART_BRR)
Note: The baud counters stop counting if the TE or RE bits are disabled respectively.