2021-06-02 08:57 PM
Ok, I scratched my head long enough and now my hope lies with the ST Community.
I would like to understand how this code in the header file stm32f1xx_ll_gpio.h works. In particular, what does (Pin >> 24) do? I suspect that the code sets two registers: GPIOx_BSRR and GPIOx_CRL. Here:
Pin = LL_GPIO_PIN_5
GPIOx = GPIOC
Thank you.
__STATIC_INLINE void LL_GPIO_SetPinMode(GPIO_TypeDef *GPIOx, uint32_t Pin, uint32_t Mode)
{
register uint32_t *pReg = (uint32_t *)((uint32_t)(&GPIOx->CRL) + (Pin >> 24));
MODIFY_REG(*pReg, ((GPIO_CRL_CNF0 | GPIO_CRL_MODE0) << (POSITION_VAL(Pin) * 4U)),
Mode << (POSITION_VAL(Pin) * 4U)));
}
Solved! Go to Solution.
2021-06-02 09:09 PM
The 26th bit is 1 for pins 8 and higher which makes the code set pReg to point to GPIOx->CRH rather than GPIOx->CRL.
#define LL_GPIO_PIN_0 ((GPIO_BSRR_BS0 << GPIO_PIN_MASK_POS) | 0x00000001U) /*!< Select pin 0 */
#define LL_GPIO_PIN_1 ((GPIO_BSRR_BS1 << GPIO_PIN_MASK_POS) | 0x00000002U) /*!< Select pin 1 */
#define LL_GPIO_PIN_2 ((GPIO_BSRR_BS2 << GPIO_PIN_MASK_POS) | 0x00000004U) /*!< Select pin 2 */
#define LL_GPIO_PIN_3 ((GPIO_BSRR_BS3 << GPIO_PIN_MASK_POS) | 0x00000008U) /*!< Select pin 3 */
#define LL_GPIO_PIN_4 ((GPIO_BSRR_BS4 << GPIO_PIN_MASK_POS) | 0x00000010U) /*!< Select pin 4 */
#define LL_GPIO_PIN_5 ((GPIO_BSRR_BS5 << GPIO_PIN_MASK_POS) | 0x00000020U) /*!< Select pin 5 */
#define LL_GPIO_PIN_6 ((GPIO_BSRR_BS6 << GPIO_PIN_MASK_POS) | 0x00000040U) /*!< Select pin 6 */
#define LL_GPIO_PIN_7 ((GPIO_BSRR_BS7 << GPIO_PIN_MASK_POS) | 0x00000080U) /*!< Select pin 7 */
#define LL_GPIO_PIN_8 ((GPIO_BSRR_BS8 << GPIO_PIN_MASK_POS) | 0x04000001U) /*!< Select pin 8 */
#define LL_GPIO_PIN_9 ((GPIO_BSRR_BS9 << GPIO_PIN_MASK_POS) | 0x04000002U) /*!< Select pin 9 */
#define LL_GPIO_PIN_10 ((GPIO_BSRR_BS10 << GPIO_PIN_MASK_POS) | 0x04000004U) /*!< Select pin 10 */
#define LL_GPIO_PIN_11 ((GPIO_BSRR_BS11 << GPIO_PIN_MASK_POS) | 0x04000008U) /*!< Select pin 11 */
#define LL_GPIO_PIN_12 ((GPIO_BSRR_BS12 << GPIO_PIN_MASK_POS) | 0x04000010U) /*!< Select pin 12 */
#define LL_GPIO_PIN_13 ((GPIO_BSRR_BS13 << GPIO_PIN_MASK_POS) | 0x04000020U) /*!< Select pin 13 */
#define LL_GPIO_PIN_14 ((GPIO_BSRR_BS14 << GPIO_PIN_MASK_POS) | 0x04000040U) /*!< Select pin 14 */
#define LL_GPIO_PIN_15 ((GPIO_BSRR_BS15 << GPIO_PIN_MASK_POS) | 0x04000080U) /*!< Select pin 15 */
2021-06-02 09:09 PM
The 26th bit is 1 for pins 8 and higher which makes the code set pReg to point to GPIOx->CRH rather than GPIOx->CRL.
#define LL_GPIO_PIN_0 ((GPIO_BSRR_BS0 << GPIO_PIN_MASK_POS) | 0x00000001U) /*!< Select pin 0 */
#define LL_GPIO_PIN_1 ((GPIO_BSRR_BS1 << GPIO_PIN_MASK_POS) | 0x00000002U) /*!< Select pin 1 */
#define LL_GPIO_PIN_2 ((GPIO_BSRR_BS2 << GPIO_PIN_MASK_POS) | 0x00000004U) /*!< Select pin 2 */
#define LL_GPIO_PIN_3 ((GPIO_BSRR_BS3 << GPIO_PIN_MASK_POS) | 0x00000008U) /*!< Select pin 3 */
#define LL_GPIO_PIN_4 ((GPIO_BSRR_BS4 << GPIO_PIN_MASK_POS) | 0x00000010U) /*!< Select pin 4 */
#define LL_GPIO_PIN_5 ((GPIO_BSRR_BS5 << GPIO_PIN_MASK_POS) | 0x00000020U) /*!< Select pin 5 */
#define LL_GPIO_PIN_6 ((GPIO_BSRR_BS6 << GPIO_PIN_MASK_POS) | 0x00000040U) /*!< Select pin 6 */
#define LL_GPIO_PIN_7 ((GPIO_BSRR_BS7 << GPIO_PIN_MASK_POS) | 0x00000080U) /*!< Select pin 7 */
#define LL_GPIO_PIN_8 ((GPIO_BSRR_BS8 << GPIO_PIN_MASK_POS) | 0x04000001U) /*!< Select pin 8 */
#define LL_GPIO_PIN_9 ((GPIO_BSRR_BS9 << GPIO_PIN_MASK_POS) | 0x04000002U) /*!< Select pin 9 */
#define LL_GPIO_PIN_10 ((GPIO_BSRR_BS10 << GPIO_PIN_MASK_POS) | 0x04000004U) /*!< Select pin 10 */
#define LL_GPIO_PIN_11 ((GPIO_BSRR_BS11 << GPIO_PIN_MASK_POS) | 0x04000008U) /*!< Select pin 11 */
#define LL_GPIO_PIN_12 ((GPIO_BSRR_BS12 << GPIO_PIN_MASK_POS) | 0x04000010U) /*!< Select pin 12 */
#define LL_GPIO_PIN_13 ((GPIO_BSRR_BS13 << GPIO_PIN_MASK_POS) | 0x04000020U) /*!< Select pin 13 */
#define LL_GPIO_PIN_14 ((GPIO_BSRR_BS14 << GPIO_PIN_MASK_POS) | 0x04000040U) /*!< Select pin 14 */
#define LL_GPIO_PIN_15 ((GPIO_BSRR_BS15 << GPIO_PIN_MASK_POS) | 0x04000080U) /*!< Select pin 15 */
2021-06-02 10:21 PM
2021-06-02 10:27 PM