2020-09-16 7:35 PM
I'm not sure how I did it, but my Blue Pill STM32F103C8T6 doesn't respond to st-info --probe any more. This has happened twice in a row with identical devices. It seems that if I Ctrl-D out of GDB (an old bad habit) the device seems to brick itself and won't respond to programming or STLINK probes. I'm using an STLINK/V2 programmer attached to the SWIO/SWCLK pins.
I can still set the BOOT0 pin to boot the system ROM bootloader and get proper responses from the STLINK/V2 programmer. So, I'm wondering where I can download the original flash bootloader and what address I'd need to use with st-flash to flash it back onto the device so that I can return to a nice wholesome flash bootloader.
2020-09-16 7:45 PM
https://www.instructables.com/id/Programming-STM32-Blue-Pill-Via-USB/
https://github.com/rogerclarkmelbourne/Arduino_STM32/wiki/Flashing-Bootloader-for-BluePill-Boards
2020-09-16 8:08 PM
I mean these are both respectable USB bootloaders but the original flash bootloader that I had was just an STLINK/V2 over SWD programmer. Do you know if that is available for download?
2020-09-17 2:50 AM
Look on github
2023-04-30 7:07 AM
I'm facing the same issue.
The ST-link want respond. but the code uploads over uart
2023-04-30 8:39 AM
>I'm facing the same issue.
really ?
i didnt see any specification , what "original" bootloader he is talking about...you can tell this ?
is it arduino ???
2023-04-30 8:49 AM
No you're here with a "Me Too" issue 3 years later
The Blue-Pill board does not include an ST-LINK, you'll always get an "ST-LINK Not Found" type error with them. STM32 Cube Programmer can connect via USART/COM methods.
What "errors" specifically are you getting?
There are precompiled binaries for the code reside ON the Blue-Pill board that are called out on the pages already cited.
https://github.com/rogerclarkmelbourne/STM32duino-bootloader/tree/master/binaries
https://github.com/rogerclarkmelbourne/Arduino_STM32/wiki/Flashing-Bootloader-for-BluePill-Boards