2018-08-14 6:32 AM
What I do now:
And just build it and flash it. The only COM port I saw it's ST-Link (com3)
As sanity check: usb cabel connected to both usb_connectors on board (not only to ST-Link micro usb) after connecting usb to main part of the board LD8 (green) lights up.
The blinking blue led just for debugging purposes, to make sure that board was flashed.
But I don't see another COM port into device manager, only the ST-link one:
Solved! Go to Solution.
2018-08-17 6:12 AM
Hello @esukh ,
Please make sure to increase the heap size.Using Keil for example, the heap size is 0x200 by default which is too low for USB applications.
Khouloud.
2018-08-14 6:38 AM
attachment:
2018-08-14 7:37 AM
I'd probably port
STM32Cube_FW_H7_V1.3.0\Projects\STM32H743I_EVAL\Applications\USB_Device\CDC_Standalone
Use the ST-LINK VCP to output diagnostic and telemetry information to understand if the device code is functioning or interacting with the system. Perhaps confirm if you can have it appear as a DFU device if you strap BOOT(0) High and connect.
2018-08-15 6:40 AM
I did, and my device manager discover some unknown usb device, but there is no description to it.
And this is really amaze to me, why does native example doesn't work correctly (I checked that all pins on EVAL board the same as on nucleo)
2018-08-17 6:12 AM
Hello @esukh ,
Please make sure to increase the heap size.Using Keil for example, the heap size is 0x200 by default which is too low for USB applications.
Khouloud.
2018-08-17 7:09 AM
Some other points to check:
Khouloud.
2018-08-22 5:37 AM
Thank you!
2018-08-23 2:43 AM
You're always welcome!
Khouloud.
2021-04-17 10:07 AM
Dear @esukh
did your code start to work (you start to see two COM ports: from stlink and usb CN13 ) ?
I have the same probrem - i take my Nucleo STM32H743 board, open example for STM32H743 EVAL (generated by CUBE) USB_DEVICE/CDC_STANDLONE from STM site and program my board.
It doesn't work (
In code: "Heap_Size EQU 0x1500" "Stack_Size EQU 0x1500"
Chip is the same and i hoped, that code for EVAL board will work on NUCLEO board.
Could you explain what i need to change for: starting to see TWO com ports and code will start to work ?
My MAIN function:
unsigned char text[20]="Hello 2021";
/* Enable the CPU Cache */
CPU_CACHE_Enable();
HAL_Init();
/* Configure the system clock */
SystemClock_Config();
/* Init Device Library */
USBD_Init(&USBD_Device, &VCP_Desc, 0);
HAL_PWREx_EnableUSBVoltageDetector();
/* Add Supported Class */
USBD_RegisterClass(&USBD_Device, USBD_CDC_CLASS);
/* Add CDC Interface Class */
USBD_CDC_RegisterInterface(&USBD_Device, &USBD_CDC_fops);
/* Start Device Process */
USBD_Start(&USBD_Device);
USBD_CDC_RegisterInterface(&USBD_Device,&USBD_CDC_fops);
// my code
USBD_LL_Init(&USBD_Device); // Idecided that wiil help to send data via com port to PC
USBD_LL_DevConnected(&USBD_Device); // Idecided that wiil help to send data via com port to PC
while (1)
{
USBD_LL_Transmit(&USBD_Device,0,text, 20); // Idecided that wiil help to send data via com port to PC
// USBD_CDC_SetTxBuffer(&USBD_Device, text,20);
// USBD_CDC_TransmitPacket(&USBD_Device);
}
Best regards.