2020-01-01 7:16 AM
After some of research about SD Card integration with STM32 MCU, I realized that SDIO is the simpliest and most supported protocol between ST community. However, I've also found that there is no low power MCU which satisfy my specs:
When I tought that I had found the most fittable (STM32L431KC) MCU, STCubeMX did not let me configure SDIO interface.
Should I change SDIO interface to SPI? For what I've seen integrate STM32 MCUs with SDCard trough SPI it's challenging and can bring a lot of complications.
Any one have a good Application Note about that?
Any help would be appreciated, and an amazing new year.
2020-01-01 8:29 AM
Not sure the SPI or SDIO/SDMMC are any more or less complicated than each other, I'd lean on the SPI being simpler.
There are examples in HAL for both methods. The real issue with SPI is the inherent slowness.
As I recall the SDIO/SDMMC needs parts with at least 64-pins, definitely had both SPI and SDMMC running on an L4 Nucleo-64 board.
2020-01-01 10:40 AM
Print the datasheet io pin list. Do use SDMMC pins.
SWD = 2 specific pins
SDMMC = 6 pins + 1 leftover GPIO for detection
SAI = 4 pins
UART = 2+ pins
SPI master = 3 pins + gpio for NSS
I2C = if left, ok, otherwise, bitbanging will enhance options
The most rich pins are the ones common to all packages of a family, typically port A and B.
2020-01-07 10:07 PM
SDIO interface is faster than spi
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.