2019-05-11 03:45 AM
I try to implement AN3997 Application using cubemx. but I don't know how to configure the peripheral. no information has been given in the document. Can someone help me.
thank you
2019-05-11 08:03 AM
There's very little useful information from ST about their code examples and CubeMX, other than cryptic translated comments. If they give you a code example, they do not provide the IOC file. But yet, they want you to use...CubeMX. A conundrum, yes? Welcome to the mystery of ST club! I have never seen a project like that configured start to end in CubeMX, so it will be one you need to work through.
2019-05-11 04:59 PM
If you have downloaded the Cubemx files for F4 you will file under projects.
My path to the files are "D:\MyData\STM32\CubeF4\Projects\STM32F4-Discovery\Demonstrations\SW4STM32\STM32F4-DISCO"
Your path will be different.
If I try to open file ".project" with true studio it asks if I want to convert this file to a truestudio project. I would think CubeIDE would do the same.
2019-05-12 01:39 AM
I didn't know it was the codes for this document. Can you send me a link?
Then I can try the method you recommended.
2019-05-12 08:46 AM
If you have downloaded CubeMX for F4 then:
In CubeMX program click on ->help -> Updater Settings -> find Repository Folder
From this directory find folder STM32Cube_FW_F4_???? for projects
If you have not downloaded yet then see: