How can I block the execution of the my task in RTOS
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2021-08-19 3:36 AM
Hi,
Here i want to stop the particular task for certain time
when it receives the event from another task it should continue.
here is my code .
the task is not stopping.
can any one help me
/*----------------------------------------------------------------------------
* CMSIS-RTOS 'main' function template
*---------------------------------------------------------------------------*/
#include "RTE_Components.h"
#include CMSIS_device_header
#include "cmsis_os2.h"
#include "stm32f2xx_hal.h"
#include "main.h"
#include "stm32f2xx_hal_gpio.h"
#include "stm32f2xx_hal_usart.h"
//int Init_Thread (void);
#define FLAG_MASK 0x00000001U
osEventFlagsId_t EventFlagsId_t;
int val;
/*----------------------------------------------------------------------------
* I/O Configuration
*---------------------------------------------------------------------------*/
void gpioInitfunction(void)
{
__HAL_RCC_GPIOF_CLK_ENABLE(); // enabling the peripheral clock
// gpio structure initialization
GPIO_InitTypeDef GPIO_InitStructure;
GPIO_InitStructure.Mode= GPIO_MODE_INPUT ;
GPIO_InitStructure.Pin= GPIO_PIN_0;
GPIO_InitStructure.Pull= GPIO_PULLUP;
GPIO_InitStructure.Speed= GPIO_SPEED_FREQ_HIGH;
HAL_GPIO_Init(GPIOF, &GPIO_InitStructure);
}
/*----------------------------------------------------------------------------
* Application main thread
*---------------------------------------------------------------------------*/
__NO_RETURN static void app_main (void *argument) {
(void)argument;
while(1);
}
/*----------------------------------------------------------------------------
* Application ledBlink thread
*---------------------------------------------------------------------------*/
__NO_RETURN static void ledBlink (void *argument) {
(void)argument;
gpioInitfunction();
val=0;
/* here we are blinking the LED*/
while(1)
{
// here we need to implent the logic for the read the input from the gpio pins
if((HAL_GPIO_ReadPin(GPIOF,GPIO_PIN_0)==SET)&&(val==0))
{
val++;
val++;
osEventFlagsSet(EventFlagsId_t,FLAG_MASK);
}
}
}
/*----------------------------------------------------------------------------
* Application serialDataExcahnge thread
*---------------------------------------------------------------------------*/
__NO_RETURN static void serialDataExcahnge (void *argument) {
(void)argument;
uint8_t buff[10]="hello";
uint32_t flags;
/* enabling the peripheral clock */
__HAL_RCC_GPIOB_CLK_ENABLE();
__HAL_RCC_USART3_CLK_ENABLE();
GPIO_InitTypeDef GPIO_InitStructure;
USART_HandleTypeDef USART_HandleInit;
USART_HandleInit.Instance=USART3;
GPIO_InitStructure.Mode= GPIO_MODE_AF_PP ;
GPIO_InitStructure.Pin= GPIO_PIN_10|GPIO_PIN_11;
GPIO_InitStructure.Pull= GPIO_PULLUP;
GPIO_InitStructure.Speed= GPIO_SPEED_FREQ_HIGH;
GPIO_InitStructure.Alternate=GPIO_AF7_USART3;
HAL_GPIO_Init(GPIOB, &GPIO_InitStructure);
USART_HandleInit.Init.BaudRate=9600;
USART_HandleInit.Init.CLKLastBit=USART_LASTBIT_ENABLE;
USART_HandleInit.Init.CLKPhase=USART_PHASE_1EDGE;
USART_HandleInit.Init.CLKPolarity=USART_POLARITY_LOW;
USART_HandleInit.Init.Mode=USART_MODE_TX_RX ;
USART_HandleInit.Init.WordLength=UART_WORDLENGTH_8B;
USART_HandleInit.Init.Parity=USART_PARITY_NONE;
USART_HandleInit.Init.StopBits=USART_STOPBITS_1;
HAL_USART_Init(&USART_HandleInit);
HAL_USART_Transmit(&USART_HandleInit,buff,5,100);
while(1)
{
flags = osEventFlagsWait(EventFlagsId_t,FLAG_MASK, osFlagsWaitAny, osWaitForever);
HAL_USART_Transmit(&USART_HandleInit,buff,5,100);
osDelay(1000);
HAL_USART_Transmit(&USART_HandleInit,buff,5,100);
osDelay(1000);
val=0;
}
}
int main (void) {
// System Initialization
osThreadId_t thread_id;
SystemCoreClockUpdate();
// ...
osKernelInitialize(); // Initialize CMSIS-RTOS
EventFlagsId_t = osEventFlagsNew (NULL);
osThreadNew(app_main, NULL, NULL); // Create application main thread
thread_id = osThreadNew(ledBlink, NULL, NULL); // Create application ledBlink thread
osThreadNew(serialDataExcahnge, NULL, NULL); // Create application serialDataExcahnge thread
//Init_Thread ();
osKernelStart(); // Start thread execution
for (;;) {}
}
Solved! Go to Solution.
- Labels:
-
STM32F2 Series
Accepted Solutions
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2021-08-19 5:04 AM
I don't see any freertos thread synchronization mechanisms so I think you're not fully aware of them. I suggest to have a look to the freertos documentation (https://www.freertos.org/features.html) to see which mechanisms you could use to synchronize threads.
You could for example use a messagequeue system, or use semaphores to have the 2 threads communicate.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2021-08-19 5:04 AM
I don't see any freertos thread synchronization mechanisms so I think you're not fully aware of them. I suggest to have a look to the freertos documentation (https://www.freertos.org/features.html) to see which mechanisms you could use to synchronize threads.
You could for example use a messagequeue system, or use semaphores to have the 2 threads communicate.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2021-08-20 1:37 AM
Thanks for your help.