cancel
Showing results for 
Search instead for 
Did you mean: 

Hi,I am using the STM32H757(master) to load code into flash of another STM32H757(slave). The slave is in bootloader mode ( SPI ). Question 1: Does somebody has a driver for the master side to read/write into slave, especialy option bytes? Thank you

baptor
Associate III
 
1 REPLY 1
baptor
Associate III

Question 2 : When the Go command is issued from the master, ( set pointer to start adress of loaded code in slave), what is the core that will start from this adress ( CM4 or CM7 ) ? I dont understant how it is managed.

thank you