cancel
Showing results for 
Search instead for 
Did you mean: 

Help for STM32 F767Zi as USB host for mass storage

SBach.4
Associate II

Hi, I am using STM32 F767Zi and tried this tutorial to use it as an USB host ***. I followed the steps but I always end up in Use Case _USER_CLASS_ACTIVE. I tried different USB devices but it's always the same. Does anyone have an idea how I can solve the problem or how I can look for the problem? Thank you!

Post link deleted to adhere community guidelines.

This discussion is locked. Please start a new topic to ask your question.
1 ACCEPTED SOLUTION

Accepted Solutions
SBach.4
Associate II
4 REPLIES 4

Have ControllersTech support you?

You have a NUCLEO-F767ZI board OR you have a STM32F767I chip on some other board?

Perhaps look a available USB MSC HOST code in theCubeF7 repository for NUCLEO, DISCO, EVAL boards?

STM32Cube_FW_F7_V1.15.0\Projects\STM32F767ZI-Nucleo\Applications\USB_Host\MSC_Standalone

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
SBach.4
Associate II

Thank you very much for your answer!

No I just used the tutorial of ControllersTech to set up the project.

I have the Nucleo-F767ZI board.

I am so sorry I have to ask, but I can not figure it out; how do I implement the sample code from CubeF7 into Cube Ide?

Pavel A.
Evangelist III

> how do I implement the sample code from CubeF7 into Cube Ide?

Just use the CubeIDE feature, "import example project". Read the fine CubeIDE manual for details. Make sure to update CubeIDE and the CubeFW_F7 package.

SBach.4
Associate II