cancel
Showing results for 
Search instead for 
Did you mean: 

Hello, Is there an example for the STM32H7 ETH HAL V11.0 (new reworked ETH driver) without the LWIP. All the example i found are coupled with the LWIP. Thanks.

FB__1
Associate III

Following function are tied to the LWIP functions and i do not want to use any LWIP etc...

How to bypass that ?

void HAL_ETH_RxAllocateCallback(uint8_t **buff)
{
  struct pbuf_custom *p = LWIP_MEMPOOL_ALLOC(RX_POOL);
  if (p)
  {
    /* Get the buff from the struct pbuf address. */
    *buff = (uint8_t *)p + offsetof(RxBuff_t, buff);
    p->custom_free_function = pbuf_free_custom;
    /* Initialize the struct pbuf.
    * This must be performed whenever a buffer's allocated because it may be
    * changed by lwIP or the app, e.g., pbuf_free decrements ref. */
    pbuf_alloced_custom(PBUF_RAW, 0, PBUF_REF, p, *buff, ETH_RX_BUFFER_SIZE);
  }
  else
  {
    RxAllocStatus = RX_ALLOC_ERROR;
    *buff = NULL;
  }
}
 
void HAL_ETH_RxLinkCallback(void **pStart, void **pEnd, uint8_t *buff, uint16_t Length)
{
  struct pbuf **ppStart = (struct pbuf **)pStart;
  struct pbuf **ppEnd = (struct pbuf **)pEnd;
  struct pbuf *p = NULL;
 
  /* Get the struct pbuf from the buff address. */
  p = (struct pbuf *)(buff - offsetof(RxBuff_t, buff));
  p->next = NULL;
  p->tot_len = 0;
  p->len = Length;
 
  /* Chain the buffer. */
  if (!*ppStart)
  {
    /* The first buffer of the packet. */
    *ppStart = p;
  }
  else
  {
    /* Chain the buffer to the end of the packet. */
    (*ppEnd)->next = p;
  }
  *ppEnd  = p;
 
  /* Update the total length of all the buffers of the chain. Each pbuf in the chain should have its tot_len
   * set to its own length, plus the length of all the following pbufs in the chain. */
  for (p = *ppStart; p != NULL; p = p->next)
  {
    p->tot_len += Length;
  }
 
  /* Invalidate data cache because Rx DMA's writing to physical memory makes it stale. */
  SCB_InvalidateDCache_by_Addr((uint32_t *)buff, Length);
}
 
void HAL_ETH_TxFreeCallback(uint32_t * buff)
{
  pbuf_free((struct pbuf *)buff);
}
 

This discussion is locked. Please start a new topic to ask your question.
1 ACCEPTED SOLUTION

Accepted Solutions
Pavel A.
Super User

ST offers Azure RTOS integration for STM32H7, so there are examples for the ThreadX network stack (NetX).

View solution in original post

2 REPLIES 2
Pavel A.
Super User

ST offers Azure RTOS integration for STM32H7, so there are examples for the ThreadX network stack (NetX).

Thank you. I will give it a try...