Skip to main content
HanCheng Liu
Visitor II
October 22, 2017
Question

HAL_UART_Transmit_DMA() only work one time

  • October 22, 2017
  • 3 replies
  • 2460 views
Posted on October 22, 2017 at 16:13

I want to use  ' HAL_UART_Transmit_DMA(); ' to send data in DMA mode like this :

    char str_Hello[]='Hello\n';

    HAL_UART_Transmit_DMA(&huart1,(unsigned char *)str_Hello,strlen(str_Hello));

    HAL_Delay(500);

But transimit function only work one time(DMA is working under normal mode).

I found these in the definition of function 'HAL_UART_Transmit_DMA()' in 'stm32f1xx_hal_uart.c'

HAL_StatusTypeDef HAL_UART_Transmit_DMA(UART_HandleTypeDef *huart, uint8_t *pData, uint16_t Size)

{

  uint32_t *tmp;

  /* Check that a Tx process is not already ongoing */

  if(huart->gState == HAL_UART_STATE_READY)

{

......

huart->gState = HAL_UART_STATE_BUSY_TX;

.....

}

}

So, I try to manually set 'huart->gState' in my while loop like this

  char str_Hello[]='Hello\n';

  HAL_UART_Transmit_DMA(&huart1,(unsigned char *)str_Hello,strlen(str_Hello));

  HAL_Delay(500);

  huart1.gState = HAL_UART_STATE_READY

Although the problem was solved , but i think that it may not the correct way to solve this issue.

Anyone know how to handle it?

Thanks.

#uart #dma #hal #stm32f1
This topic has been closed for replies.

3 replies

Tesla DeLorean
Guru
August 10, 2018

Sorry, bumping old zombie unanswered threads off my feed

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
gilramon
Associate II
January 11, 2024

It's because you forgot to enable the interrupt of the UART that you work with in Cubemx.

Karl Yamashita
Principal
January 11, 2024

Did you assign a DMA channel to the Tx? 

 

Edit: Dang this is an old thread, lol.

If a reply has proven helpful, click on Accept as Solution so that it'll show at top of the post.CAN Jammer an open source CAN bus hacking toolCANableV3 Open Source