cancel
Showing results for 
Search instead for 
Did you mean: 

HAL_OSPI_Command_IT vs HAL_OSPI_Command, when cmd->DataMode != HAL_OSPI_DATA_NONE

Aleks
Associate III

Hi, dear colleagues!

I use OSPI interface to connect MCU with QSPI NAND flash.

For some commands (for ex. PAGE READ) of used NAND device there is 0 data bytes and HAL_OSPI_Command_IT() work proper.

But some commands (for ex. SET FEATURE) has one (or more) data bytes. With those commands HAL_OSPI_Command_IT() fail (return HAL_ERROR). It is obviously also when view HAL_OSPI_Command_IT source code - it can't be used for commands with non zero data bytes , i.e DataMode != HAL_OSPI_DATA_NONE.

But HAL_OSPI_Command() do this OK.

I use both functions with the same hospi and cmd configuration, but HAL_OSPI_Command_IT() is failed, HAL_OSPI_Command() is OK.

Is there difference in purpouse of HAL_OSPI_Command_IT and HAL_OSPI_Command?

Is there any restrictions for HAL_OSPI_Command_IT vs HAL_OSPI_Command?

Thank you.

This discussion is locked. Please start a new topic to ask your question.
0 REPLIES 0