HAL_NOR_MspWait implementation
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2017-03-13 7:44 AM
Hello
I generated a project with Stm32CubeMX with a NOR Flash connected in the FSMC. This NOR Flash has a Ready/Busy signal and the HAL NOR has a function to handle this signal: HA_NOR_MspWait. What can I do, if I want to implement this function without modifying the stm32f4xx_hal_nor.c file?Best regards!
#fsmc-nor #hal- Labels:
-
FMC-FSMC
-
STM32Cube MCU Packages
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2017-03-13 2:45 PM
> This NOR Flash has a Ready/Busy signal
Can you give a link to its datasheet?
I don't Cube so I don't know how to do this in that environment, but generally you enable the asynchronous WAIT using ASYNCWAIT bit in the respective FSMC_BCRx register. There are several timing considerations which go with this bit, read the WAIT management in asynchronous accesses subchapter of FSMC chapter. And of course, don't forget to connect the NWAIT pin and set it up as appropriate AF in GPIO.
JW
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2017-03-14 2:37 AM
Hi waclawek.jan
the datasheet Flash memory is
(S29GL128S). My current MCU is a SMT32F429 with a LCD. The NWAIT's pin is used by the LCD_B2 function of LCD's driver . RY/BY's signal is connected to PC13 (This pin hasn't an alternative function). My idea is manage the wait procedure implementing the HAL_NOR_MspWait function.
In the STM32F10x_StdExamples, there is an example of FSMC NOR without HAL implementation and the management of RD/BY signal. I think in my case, my HAL_NOR_MspWait has contain a code something like this:NOR_Status NOR_GetStatus(uint32_t Timeout)
{
uint16_t val1 = 0x00, val2 = 0x00;
NOR_Status status = NOR_ONGOING;
uint32_t timeout = Timeout;
/*!< Poll on NOR memory Ready/Busy signal ----------------------------------*/
while((GPIO_ReadInputDataBit(GPIOD, GPIO_Pin_6) != RESET) && (timeout > 0))
{
timeout--;
}
timeout = Timeout;
while((GPIO_ReadInputDataBit(GPIOD, GPIO_Pin_6) == RESET) && (timeout > 0))
{
timeout--;
}
...
}
Best regards