Skip to main content
chief
Associate II
March 30, 2015
Question

HAL_FLASH_Program always return error code 0x06

  • March 30, 2015
  • 2 replies
  • 1049 views
Posted on March 30, 2015 at 15:44

I use STM32F417IG

Minimal example of code:

uint32_t startAddress = 0x80E0000;

static uint32_t mSize =0x13;//

char test_string[13]={''Hello World.''};

HAL_FLASH_Unlock();

for(uint32_t i=0;i<mSize;i++)

{

status = HAL_FLASH_Program(FLASH_TYPEPROGRAM_BYTE, startAddress+i,test_string[i]);

if(status==HAL_ERROR)

{

printf(''Flash error code: %d for data index %d\n'',HAL_FLASH_GetError(),i);//Always return 6

}

}

What is wrong?

#flash #hal #stm32
This topic has been closed for replies.

2 replies

Tesla DeLorean
Guru
March 30, 2015
Posted on March 30, 2015 at 21:24

Dunno, what's 6 defined as meaning, and is the memory erased, check the bytes are 0xFF

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
chief
chiefAuthor
Associate II
March 31, 2015
Posted on March 31, 2015 at 07:11

#define HAL_FLASH_ERROR_PGS          ((uint32_t)0x00000002)    /*!< Programming Sequence error    */

#define HAL_FLASH_ERROR_PGP          ((uint32_t)0x00000004)    /*!< Programming Parallelism error */

Sector 12 (0x080E000 - 0x080FFFFF) filed by 0xff. I try to fully erase chip by j-link flashing device. No any changes.