2021-07-18 5:20 AM
Hi,
i had a working STM32F1 (BluePill) CAN-Node with Cube firmware V1.8.0 before STMCube suggested me to automatically migrate the firmware to the latest V1.8.4.
Now HAL_CAN_Init() returns with an error which is caused by this code part within the Cube generated init function:
/* Wait initialisation acknowledge */
while ((hcan->Instance->MSR & CAN_MSR_INAK) == 0U)
{
if ((HAL_GetTick() - tickstart) > CAN_TIMEOUT_VALUE)
{
/* Update error code */
hcan->ErrorCode |= HAL_CAN_ERROR_TIMEOUT;
/* Change CAN state */
hcan->State = HAL_CAN_STATE_ERROR;
return HAL_ERROR;
}
}
obviously the "CAN_MSR_INAK" -bit in the MSR-register does not get set.
While testing the MCU is connected via TJA1050 tranceiver to a working can network.
Does anyone else encounter this problem ?
2022-03-05 11:53 PM
Modifying the code in this way seems to be working:
/* Request initialisation */
SET_BIT(hcan->Instance->MCR, CAN_MCR_INRQ);
/* Exit from sleep mode */
CLEAR_BIT(hcan->Instance->MCR, CAN_MCR_SLEEP);
/* Get tick */
tickstart = HAL_GetTick();
/* Wait initialisation acknowledge */
while ((hcan->Instance->MSR & CAN_MSR_INAK) == 0U)
{
if ((HAL_GetTick() - tickstart) > CAN_TIMEOUT_VALUE)
{
/* Update error code */
hcan->ErrorCode |= HAL_CAN_ERROR_TIMEOUT;
/* Change CAN state */
hcan->State = HAL_CAN_STATE_ERROR;
return HAL_ERROR;
}
}
/* Exit from sleep mode */
//CLEAR_BIT(hcan->Instance->MCR, CAN_MCR_SLEEP); COMMENTED OUT
/* Get tick */
tickstart = HAL_GetTick();
/* Check Sleep mode leave acknowledge */
while ((hcan->Instance->MSR & CAN_MSR_SLAK) != 0U)
Nevertheless, if you look into 1.8.3 the two sections of code (i.e. "Exit from sleep mode" and "Request initialization") are reversed - with "Exit from sleep mode" being put first and only after "Request initialization" comes.