2020-11-29 7:51 AM
In STUSB4500 datasheet, it says below for ALERT pin:
Pin 19, B2, ALERT, OD, I2C interrupt, active low open drain, To I2C master, ext. pull-up.
What does it mean - is the signal triggered when I2C command is sent from I2C master to STUSB4500?
Thanks,
Winston
2020-12-02 5:10 AM
ALERT is a signal from the STUSB4500 to the master and signals some transmission. You will also find it in the libraries, e.g. STSW-STUSB003.
When your question is answered, please close this topic by choosing Select as Best.
Regards
/Peter
2020-12-02 2:32 PM
Hi Peter,
Thanks for the answer. I have read the STW-STUSB003 but it does not give a hint as to when the signal will be sent.
That is what I want to know: can you give me some examples as to what transmission is signaled? Will the signal be sent once for each I2C transaction?
Thanks,
Winston
2020-12-03 6:23 AM
Hi Winston,
ALERT pin is not triggered I2C events but functional events. In the STSW-STUSB003 package, you can find a DOC directory which contains the product register map. ALERT pin behaviour can be configured by masking/unmasking relevant events or interrupts according to your application requirements. See ALERT_STATUS registers and similar @ 0x0B, 0x0C etc...
Hope it helps,
Rgds,
Benoit
2022-04-07 4:22 PM
@Benoit FORET Why has the datasheet not been updated to include the functional description this pin?
2022-04-14 7:54 AM
Hi. Thanks for your suggestion.
So far, this is a choice we made to document software related features in a separate section.
Rgds