Hi Sahin,understand your request, but to achieve fast enough voltage transition (according to USB PD requirements), an interrupt and a dedicated register map are required to quickly drive the Buck-Boost according to USB PD negotiation. While this IC ...
Hi,STUSB4761 has been optimized for AC/DC applications: Voltage and Current are regulated directly through analog signals. With some compliant DC/DC, OPTO_DRV and FB pins can be used similarly to set the regulation point, but I understand it might no...
Hello,STSW-STUSB003 is a software library to be used for dynamic power profile modification, and it is not saving permanently the configuration indeed.But from st.com, you can also download a utility called STSW-STUSB004, to be used to translate the ...
Hi KMew,your understanding is correct. This is the default configuration that is set in ST plant, ready to use for compatible 45W applications.Rgds,Benoit