cancel
Showing results for 
Search instead for 
Did you mean: 

FMC initialising and RTC desactivation

HamedAth
Visitor

 Dear All, 

I designed a HMI board with STM32F767 and QSPI NOR flash and MT48LC16M SDRAM with external OSC 8MHz and MC-306 32.768 KHz.

Approximately I tested more than 100 PCs of this board and all work without any problem. 

but during this week in some new boards, I saw when I initialise FMC, the RTC does not work anymore. even with RTC again initialising, it still doesn’t work and need to get restarted or power off. 
I also tested with internal LSI but nothing changes. I also connected V BAT to VDD the problem is still there. 
funny thing that this software works in many of these boards, but some of them have exactly the same problem.
I also removed the SDRAM and NoR flash chips, but again had same problem. 
Any body have had this problem? 

0 REPLIES 0