cancel
Showing results for 
Search instead for 
Did you mean: 

Execution delay different for NUCLEO-F207 and NUCLEO-F767 boards for the same set of lines

Shubhamkeshari
Associate III

Hi, I wrote a standard (DFT)Discreate fourier transform code (code is not the issue), in NUCLEO-F207 board using zephyr RTOS. I build the same program for NUCLEO-F767 board and flashed.

The time taken to execute DFT code in NUCLEO-F207 was 8700 micro seconds.

The time taken to execute the same code in NUCLEO-F767 is 65000 micro seconds.

FPU(Floating point unit) is enabled for NUCELO-F767 board 

Hardware and softwares are completely same for both the boards

How is it happening what is the potential cause ?

1 ACCEPTED SOLUTION

Accepted Solutions

Hello,

I don't know about that Zephyr environment. 

But you need to refer to our documentation: Especially the AN4667 "STM32F7 Series system architecture and performance".

In the HAL examples, to enable the data and the instruction cache:

static void CPU_CACHE_Enable(void) { /* Enable I-Cache */ SCB_EnableICache(); /* Enable D-Cache */ SCB_EnableDCache(); }

 For ART it is enabled in HAL_Init():

HAL_StatusTypeDef HAL_Init(void) { /* Configure Instruction cache through ART accelerator */ #if (ART_ACCELERATOR_ENABLE != 0) __HAL_FLASH_ART_ENABLE(); #endif /* ART_ACCELERATOR_ENABLE */

  So you need to check in the Zephyr environment where to enable all these features.

To give better visibility on the answered topics, please click on "Accept as Solution" on the reply which solved your issue or answered your question.

View solution in original post

9 REPLIES 9
Andrew Neil
Super User

@Shubhamkeshari wrote:

Hardware and softwares are completely same for both the boards


Hardly: they are different MCUs Cortex-M3 and -M7!

Are you sure that the optimisation level is the same on both?

What about clocking?

 


@Shubhamkeshari wrote:

FPU(Floating point unit) is enabled for NUCELO-F767 board 


So what happens if you disable it?

A complex system that works is invariably found to have evolved from a simple system that worked.
A complex system designed from scratch never works and cannot be patched up to make it work.
mÆŽALLEm
ST Employee

Hello,

As you are measuring the exec duration based on the time, need to check the System frequency first. 

Did you enable the cache/ART accelerator on the F7 product?

To give better visibility on the answered topics, please click on "Accept as Solution" on the reply which solved your issue or answered your question.

Are you sure that the optimisation level is the same on both?

- Yes same optimization level is maintained

 

What about clocking?

- NUCLEO-F767

&clk_hse {

hse-bypass;

clock-frequency = <DT_FREQ_M(8)>; /* STLink 8MHz clock */

status = "okay";

};

 

&pll {

div-m = <4>;

mul-n = <216>;

div-p = <2>;

div-q = <9>;

clocks = <&clk_hse>;

status = "okay";

};

 

&rcc {

clocks = <&pll>;

clock-frequency = <DT_FREQ_M(216)>;

ahb-prescaler = <1>;

apb1-prescaler = <4>;

apb2-prescaler = <2>;

};

 

- NUCLEO-F207

&clk_hse {
hse-bypass;
clock-frequency = <DT_FREQ_M(8)>; /* STLink 8MHz clock */
status = "okay";
};

&pll {
div-m = <8>;
mul-n = <240>;
div-p = <2>;
div-q = <5>;
clocks = <&clk_hse>;
status = "okay";
};

&rcc {
clocks = <&pll>;
clock-frequency = <DT_FREQ_M(120)>;
ahb-prescaler = <1>;
apb1-prescaler = <4>;
apb2-prescaler = <2>;
};

 

If I disable the floating point unit in NUCLEO-F767 the delay increases

No i have not enabled cache/ART accelerator , how to enable that ?

Please see: How to insert source code.

A complex system that works is invariably found to have evolved from a simple system that worked.
A complex system designed from scratch never works and cannot be patched up to make it work.

What is the environment are you using? Seems it's not a ST environment!

To give better visibility on the answered topics, please click on "Accept as Solution" on the reply which solved your issue or answered your question.

I am using Zephyr RTOS

Shubhamkeshari
Associate III
/*NUCLEO-F207*/ &clk_hse { hse-bypass; clock-frequency = <DT_FREQ_M(8)>; /* STLink 8MHz clock */ status = "okay"; }; &pll { div-m = <8>; mul-n = <240>; div-p = <2>; div-q = <5>; clocks = <&clk_hse>; status = "okay"; }; &rcc { clocks = <&pll>; clock-frequency = <DT_FREQ_M(120)>; ahb-prescaler = <1>; apb1-prescaler = <4>; apb2-prescaler = <2>; }; /*NUCLEO-F767*/ &clk_hse { hse-bypass; clock-frequency = <DT_FREQ_M(8)>; /* STLink 8MHz clock */ status = "okay"; }; &pll { div-m = <4>; mul-n = <216>; div-p = <2>; div-q = <9>; clocks = <&clk_hse>; status = "okay"; }; &rcc { clocks = <&pll>; clock-frequency = <DT_FREQ_M(216)>; ahb-prescaler = <1>; apb1-prescaler = <4>; apb2-prescaler = <2>; };
View more

Hello,

I don't know about that Zephyr environment. 

But you need to refer to our documentation: Especially the AN4667 "STM32F7 Series system architecture and performance".

In the HAL examples, to enable the data and the instruction cache:

static void CPU_CACHE_Enable(void) { /* Enable I-Cache */ SCB_EnableICache(); /* Enable D-Cache */ SCB_EnableDCache(); }

 For ART it is enabled in HAL_Init():

HAL_StatusTypeDef HAL_Init(void) { /* Configure Instruction cache through ART accelerator */ #if (ART_ACCELERATOR_ENABLE != 0) __HAL_FLASH_ART_ENABLE(); #endif /* ART_ACCELERATOR_ENABLE */

  So you need to check in the Zephyr environment where to enable all these features.

To give better visibility on the answered topics, please click on "Accept as Solution" on the reply which solved your issue or answered your question.