2023-05-11 5:46 AM
Hello everyone
Does anyone have example code for Azure RTOS USBX device class video (UVC)?
I was able to add Video to my USBX demo application on Nucleo H7A3
There was sample code for CDC_ACM and MSC (mass storage), this worked fine. But for device class video, I was not able to find any example code.
CubeIDE 1.12.1 generated two files
ux_device_video.c
ux_device_video.h
But both files only contain prototypes of callback functions which need to be filled
Like this:
/**
* @brief USBD_VIDEO_StreamRequest
* This function is invoked to manage the UVC class requests.
* @param video_stream: Pointer to video class stream instance.
* @param transfer: Pointer to the transfer request.
* @retval status
*/
UINT USBD_VIDEO_StreamRequest(UX_DEVICE_CLASS_VIDEO_STREAM *video_stream,
UX_SLAVE_TRANSFER *transfer)
{
UINT status = UX_SUCCESS;
/* USER CODE BEGIN USBD_VIDEO_StreamRequest */
UX_PARAMETER_NOT_USED(video_stream);
UX_PARAMETER_NOT_USED(transfer);
/* USER CODE END USBD_VIDEO_StreamRequest */
return status;
}How to fill it, that it works?
Thanks
Johannes
Solved! Go to Solution.
2023-05-16 12:58 AM
I got a solution.
for some bizare unknown reason, it works if I change the order of the device classes.
If I change the enumeration of the device classes, so Video comes first, it works.
uint8_t UserClassInstance[USBD_MAX_CLASS_INTERFACES] = {
CLASS_TYPE_VIDEO,
CLASS_TYPE_MSC,
CLASS_TYPE_CDC_ACM,
};Now I have a compound device with
If anyone can explain, why that is, ... highly appreciated.
Johannes
2023-05-16 1:52 AM
Hi @Johannes, as i see in your project app_usbx_device.c Tx Fifo of endpoint 4 ( EP video IN) is missed, you can see in referance project
2023-05-16 2:43 AM
Hi @Johannes , As i see in your project TxFifo Config of endpoint video (EP 4 - IN) is missed, you can check it in reference application:
2023-05-16 3:02 AM
@mohamed.ayed : I must admit, I don't understand:
If I have 4 endpoints (IN) I need one TX fifo for each endpoint?
How do these fifo indexes correspond to the endpoints?
HAL_PCDEx_SetTxFiFo(&hpcd_USB_OTG_HS, 0, 0x10);
/* Set Tx FIFO 2 */
HAL_PCDEx_SetTxFiFo(&hpcd_USB_OTG_HS, 1, 0x10);
/* Set Tx FIFO 3 */
HAL_PCDEx_SetTxFiFo(&hpcd_USB_OTG_HS, 2, 0x20);
/* Set Tx FIFO 4 */
HAL_PCDEx_SetTxFiFo(&hpcd_USB_OTG_HS, 3, 0x80);
2023-05-16 4:10 AM
in your project there is 5 endpoint IN and 3 endpoint OUT you can see it in ux_device_descriptor.h
endpoint IN
endpoint OUT
endpoint 1 and endpoint 3 is bidirectional
So for OUT endpoint size is regrouped in RxFiFo:
HAL_PCDEx_SetRxFiFo(&hpcd_USB_OTG_HS, 0x200);For IN endpoint size TxFiFo:
HAL_PCDEx_SetTxFiFo(&hpcd_USB_OTG_HS, 0, 0x10);
HAL_PCDEx_SetTxFiFo(&hpcd_USB_OTG_HS, 1, 0x10);
HAL_PCDEx_SetTxFiFo(&hpcd_USB_OTG_HS, 2, 0x20);
HAL_PCDEx_SetTxFiFo(&hpcd_USB_OTG_HS, 4, 0x80);please note that real value is multiplied x4
for example for RxFifo we have 0x200 so value is 512 *4 = 2048
In HS mode size of PCD USB fifo (sum of fifo value) sould be < 4096
2023-05-16 6:16 AM
@mohamed.ayed : thank you for explaining.
Sorry, but I am still confused.
I have 5 IN-endpoints. So I need 5 TX Fifos?
does the Fifo number in HAL_PCDEx_setTxFifo have to match the endpoint number?
HAL_PCDEx_SetTxFiFo(&hpcd_USB_OTG_HS, 0, 0x10); //->0x80
HAL_PCDEx_SetTxFiFo(&hpcd_USB_OTG_HS, 1, 0x10); //->0x81
HAL_PCDEx_SetTxFiFo(&hpcd_USB_OTG_HS, 2, 0x20); //->0x82
HAL_PCDEx_SetTxFiFo(&hpcd_USB_OTG_HS, 3, 0x20); //->0x83
HAL_PCDEx_SetTxFiFo(&hpcd_USB_OTG_HS, 4, 0x80); //->0x84Thank you for your help
Johannes
2023-05-16 6:24 AM
I tried to more TX fifos like described above. This does not solve the problem with the video device.
I still need to move the video endpoint to the top of the list of endpoint descriptors to make it work
uint8_t UserClassInstance[USBD_MAX_CLASS_INTERFACES] = {
CLASS_TYPE_VIDEO,
CLASS_TYPE_MSC,
CLASS_TYPE_CDC_ACM,
};
2023-05-16 6:31 AM
@Johannes Yes, if you see HAL_PCDEx_SetTxFiFo API description fifo parameter (The number of Tx fifo), this is the endpoint Number .
Regards,
Mohamed
2023-05-30 11:55 PM
I was able to implement the video demo
into my code using Nucleo H7A3
Does anyone know, how the demo data for the video is generated or encoded?
see file "stream1.h"
Are these "just" JPEG images put into a sequence of 28 images?
const uint8_t *tImagesList[] = {image0, image1, image2, image3, image4, image5, image6, image7, image8, image9, \
image10, image11, image12, image13, image14, image15, image16, image17, \
image18, image19, image20, image21, image22, image23, image24, image25, \
image26, image27, image28};
uint16_t tImagesSizes[] = {JPEG0_SIZE, JPEG1_SIZE, JPEG2_SIZE, JPEG3_SIZE, JPEG4_SIZE, JPEG5_SIZE, JPEG6_SIZE, \
JPEG7_SIZE, JPEG8_SIZE, JPEG9_SIZE, JPEG10_SIZE, JPEG11_SIZE, JPEG12_SIZE, \
JPEG13_SIZE, JPEG14_SIZE, JPEG15_SIZE, JPEG16_SIZE, JPEG17_SIZE, JPEG18_SIZE, \
JPEG19_SIZE, JPEG20_SIZE, JPEG21_SIZE, JPEG22_SIZE, JPEG23_SIZE, JPEG24_SIZE, \
JPEG25_SIZE, JPEG26_SIZE, JPEG27_SIZE, JPEG28_SIZE};
2023-05-31 2:13 AM
Hi @Johannes, To have encoded video.
1- split your video into images with ffmpeg libraries (see https://ffmpeg.org)
2- select your images and convert them to hex array you can use free tool for that.
BR
Mohamed