Example for Azure RTOS USBX device video (UVC)
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2023-05-11 5:46 AM
Hello everyone
Does anyone have example code for Azure RTOS USBX device class video (UVC)?
I was able to add Video to my USBX demo application on Nucleo H7A3
There was sample code for CDC_ACM and MSC (mass storage), this worked fine. But for device class video, I was not able to find any example code.
CubeIDE 1.12.1 generated two files
ux_device_video.c
ux_device_video.h
But both files only contain prototypes of callback functions which need to be filled
Like this:
/**
* @brief USBD_VIDEO_StreamRequest
* This function is invoked to manage the UVC class requests.
* @param video_stream: Pointer to video class stream instance.
* @param transfer: Pointer to the transfer request.
* @retval status
*/
UINT USBD_VIDEO_StreamRequest(UX_DEVICE_CLASS_VIDEO_STREAM *video_stream,
UX_SLAVE_TRANSFER *transfer)
{
UINT status = UX_SUCCESS;
/* USER CODE BEGIN USBD_VIDEO_StreamRequest */
UX_PARAMETER_NOT_USED(video_stream);
UX_PARAMETER_NOT_USED(transfer);
/* USER CODE END USBD_VIDEO_StreamRequest */
return status;
}
How to fill it, that it works?
Thanks
Johannes
Solved! Go to Solution.
- Labels:
-
AzureRTOS
-
STM32CubeIDE
-
STM32H7 series
-
USB
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2023-05-16 12:58 AM
I got a solution.
for some bizare unknown reason, it works if I change the order of the device classes.
If I change the enumeration of the device classes, so Video comes first, it works.
uint8_t UserClassInstance[USBD_MAX_CLASS_INTERFACES] = {
CLASS_TYPE_VIDEO,
CLASS_TYPE_MSC,
CLASS_TYPE_CDC_ACM,
};
Now I have a compound device with
- Video
- Mass storage
- virtual serial port
If anyone can explain, why that is, ... highly appreciated.
Johannes
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2023-05-16 1:52 AM
Hi @Johannes​, as i see in your project app_usbx_device.c Tx Fifo of endpoint 4 ( EP video IN) is missed, you can see in referance project
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2023-05-16 2:43 AM
Hi @Johannes​ , As i see in your project TxFifo Config of endpoint video (EP 4 - IN) is missed, you can check it in reference application:
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2023-05-16 3:02 AM
@mohamed.ayed​ : I must admit, I don't understand:
If I have 4 endpoints (IN) I need one TX fifo for each endpoint?
How do these fifo indexes correspond to the endpoints?
HAL_PCDEx_SetTxFiFo(&hpcd_USB_OTG_HS, 0, 0x10);
/* Set Tx FIFO 2 */
HAL_PCDEx_SetTxFiFo(&hpcd_USB_OTG_HS, 1, 0x10);
/* Set Tx FIFO 3 */
HAL_PCDEx_SetTxFiFo(&hpcd_USB_OTG_HS, 2, 0x20);
/* Set Tx FIFO 4 */
HAL_PCDEx_SetTxFiFo(&hpcd_USB_OTG_HS, 3, 0x80);
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2023-05-16 4:10 AM
in your project there is 5 endpoint IN and 3 endpoint OUT you can see it in ux_device_descriptor.h
endpoint IN
- endpoint 0 (mandatory for each USB device ) 0x80U
- #define USBD_MSC_EPIN_ADDR 0x81U
- #define USBD_CDCACM_EPINCMD_ADDR 0x82U
- #define USBD_CDCACM_EPIN_ADDR 0x83U
- #define USBD_VIDEO_EPIN_ADDR 0x84U
endpoint OUT
- endpoint 0 (mandatory for each USB device ) 0x00U
- #define USBD_MSC_EPOUT_ADDR 0x01U
- #define USBD_CDCACM_EPOUT_ADDR 0x03U
endpoint 1 and endpoint 3 is bidirectional
So for OUT endpoint size is regrouped in RxFiFo:
HAL_PCDEx_SetRxFiFo(&hpcd_USB_OTG_HS, 0x200);
For IN endpoint size TxFiFo:
HAL_PCDEx_SetTxFiFo(&hpcd_USB_OTG_HS, 0, 0x10);
HAL_PCDEx_SetTxFiFo(&hpcd_USB_OTG_HS, 1, 0x10);
HAL_PCDEx_SetTxFiFo(&hpcd_USB_OTG_HS, 2, 0x20);
HAL_PCDEx_SetTxFiFo(&hpcd_USB_OTG_HS, 4, 0x80);
please note that real value is multiplied x4
for example for RxFifo we have 0x200 so value is 512 *4 = 2048
In HS mode size of PCD USB fifo (sum of fifo value) sould be < 4096
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2023-05-16 6:16 AM
@mohamed.ayed​ : thank you for explaining.
Sorry, but I am still confused.
I have 5 IN-endpoints. So I need 5 TX Fifos?
does the Fifo number in HAL_PCDEx_setTxFifo have to match the endpoint number?
HAL_PCDEx_SetTxFiFo(&hpcd_USB_OTG_HS, 0, 0x10); //->0x80
HAL_PCDEx_SetTxFiFo(&hpcd_USB_OTG_HS, 1, 0x10); //->0x81
HAL_PCDEx_SetTxFiFo(&hpcd_USB_OTG_HS, 2, 0x20); //->0x82
HAL_PCDEx_SetTxFiFo(&hpcd_USB_OTG_HS, 3, 0x20); //->0x83
HAL_PCDEx_SetTxFiFo(&hpcd_USB_OTG_HS, 4, 0x80); //->0x84
Thank you for your help
Johannes
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2023-05-16 6:24 AM
I tried to more TX fifos like described above. This does not solve the problem with the video device.
I still need to move the video endpoint to the top of the list of endpoint descriptors to make it work
uint8_t UserClassInstance[USBD_MAX_CLASS_INTERFACES] = {
CLASS_TYPE_VIDEO,
CLASS_TYPE_MSC,
CLASS_TYPE_CDC_ACM,
};
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2023-05-16 6:31 AM
@Johannes​ Yes, if you see HAL_PCDEx_SetTxFiFo API description fifo parameter (The number of Tx fifo), this is the endpoint Number .
Regards,
Mohamed
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2023-05-30 11:55 PM
I was able to implement the video demo
into my code using Nucleo H7A3
Does anyone know, how the demo data for the video is generated or encoded?
see file "stream1.h"
Are these "just" JPEG images put into a sequence of 28 images?
const uint8_t *tImagesList[] = {image0, image1, image2, image3, image4, image5, image6, image7, image8, image9, \
image10, image11, image12, image13, image14, image15, image16, image17, \
image18, image19, image20, image21, image22, image23, image24, image25, \
image26, image27, image28};
uint16_t tImagesSizes[] = {JPEG0_SIZE, JPEG1_SIZE, JPEG2_SIZE, JPEG3_SIZE, JPEG4_SIZE, JPEG5_SIZE, JPEG6_SIZE, \
JPEG7_SIZE, JPEG8_SIZE, JPEG9_SIZE, JPEG10_SIZE, JPEG11_SIZE, JPEG12_SIZE, \
JPEG13_SIZE, JPEG14_SIZE, JPEG15_SIZE, JPEG16_SIZE, JPEG17_SIZE, JPEG18_SIZE, \
JPEG19_SIZE, JPEG20_SIZE, JPEG21_SIZE, JPEG22_SIZE, JPEG23_SIZE, JPEG24_SIZE, \
JPEG25_SIZE, JPEG26_SIZE, JPEG27_SIZE, JPEG28_SIZE};
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2023-05-31 2:13 AM
Hi @Johannes​, To have encoded video.
1- split your video into images with ffmpeg libraries (see https://ffmpeg.org)
2- select your images and convert them to hex array you can use free tool for that.
BR
Mohamed