2026-02-10 6:05 PM - last edited on 2026-02-11 10:19 AM by mƎALLEm
Typo fixed in title - was "Helliun"
I'm developing a project that will heavily utilize DSP for audio processing, including neural networks. However, I'm having difficulties with the DSP; I haven't finished reading all the documentation yet. I even consulted Claude Opus on the process and other AI resources, but they all point to a non-existent path, which would be to install CMSIS-DSP via CubeMX in the ARM software tree.
Is anything else needed for DSP use?
Taking advantage of this post, how should I access the board's internal microphone? Are there any code examples besides STM32N6-GettingStarted-Audio, or is that the best example to learn how to handle the microphone that comes with the board?
Thank you for your help.
2026-02-10 11:36 PM
Hello,
There us no product with part number STM32N757. I think you mean H7.
2026-02-11 1:47 AM
Did you mean Helium ?
2026-02-11 9:05 AM
Foi um erro de digitação da minha parte, é STM32N657x0.
2026-02-11 9:06 AM