cancel
Showing results for 
Search instead for 
Did you mean: 

Does STM32Cube_FW_H5_V1.2.0 MCU package suppolrt FREERTOS?

microcoder
Associate II

Greetings,

I am using a NUCLEO-H563ZI with the STM32CubeIDE, and wanted to create a new project based on 

FREERTOS. It appears that FREERTOS is not part of this release, and the tools tell me I have to download it.

1) Is there a version on FREERTOS compatible with STM32Cube_FW_H5_V1.2.0?

2) I see that STM32Cube_FW_H5_V1.2.0 supports ThreadX, is ST moving away from FREERTOS support in

favor of ThreadX?

3) How can I download and install FREERTOS into STM32Cube_FW_H5_V1.2.0?

 

Thanks

Ken

 

1 ACCEPTED SOLUTION

Accepted Solutions
STTwo-32
ST Employee

Hello @microcoder 

I suggest you to use the X-CUBE-FREERTOS. This Package is compatible with the STM32H5. If you are using CubeMX, you can directly implement FreeRTOS from the Middlewares selector. 

Best Regards.

STTwo-32 

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

View solution in original post

2 REPLIES 2
STTwo-32
ST Employee

Hello @microcoder 

I suggest you to use the X-CUBE-FREERTOS. This Package is compatible with the STM32H5. If you are using CubeMX, you can directly implement FreeRTOS from the Middlewares selector. 

Best Regards.

STTwo-32 

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

Thank you