Do the Virtual COM Port drivers work with Windows 7?
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2019-05-13 5:17 PM
I have tried installing and running projects using the USB_Device/CDC_Standalone project for both the STM32L476G-EVAL and the STM32F779I-EVAL boards, but every time I connect the board using the USB FS port, I get a driver error "This device cannot start. (Code 10)"
After uninstalling and installing the VCP drivers multiple times (using STLinkUSBDriver.dll v4.4.0.0 and Virtual COM Port driver 1.3.1.0 from VCP_V1.5.0_Setup_W7_x64_64bits.exe) , it never works. I've searched through the ST forums but have had no luck finding any documentation for this issue.
After a little more research, I found the stm32l4xx_ll_usb.c driver is hard faulting in USB_WritePacket.
The hard fault is occurring during the write of 0x200001BE USBD_StringSerial. See attached image:
I also changed the heap size according to the information in the FAQ https://community.st.com/s/article/FAQ-USB-device-not-recognized
This had no effect on the hard fault.
Solved! Go to Solution.
- Labels:
-
STM32L4 series
-
USB
Accepted Solutions
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2019-05-14 12:37 PM
Ah, the fault in USB_WritePacket.
This is simply because of unaligned 32-bit access. Already reported here earlier.
Try to change this way :
HAL_StatusTypeDef USB_WritePacket(USB_OTG_GlobalTypeDef *USBx, uint8_t *src, uint8_t ch_ep_num, uint16_t len, uint8_t dma)
{
uint32_t USBx_BASE = (uint32_t)USBx;
uint32_t *pSrc = (uint32_t *)src;
uint32_t count32b, i;
if (dma == 0U)
{
count32b = ((uint32_t)len + 3U) / 4U;
for (i = 0U; i < count32b; i++)
{
if (((uint32_t)pSrc & 0x3) == 0) {
USBx_DFIFO((uint32_t)ch_ep_num) = *((__packed uint32_t *)pSrc);
} else { //<<< UNALIGNED
uint32_t v;
memcpy(&v,pSrc,4);
USBx_DFIFO((uint32_t)ch_ep_num) = v;
}
pSrc++;
}
}
return HAL_OK;
}
(fast and dirty fix, not optimized, sorry)
-- pa
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2019-05-13 9:02 PM
Hi. Please review this thread:
and try the driver package from here:
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2019-05-14 9:41 AM
Thank you for the reply. I should have said that I have already downloaded and installed (multiple times) both the VCP driver 1.5.0 in VCP_V1.5.0_Setup_W8_x64_64bits.exe and the ST-Link driver in STSW-LINK009.
I am already running the latest drivers from ST for both ST-Link and the Virtual COM Port.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2019-05-14 11:44 AM
Looks like my problem is similar to this thread: https://community.st.com/s/question/0D50X0000Amj7LqSQI/stm32f407vgtx-cdc-error-driver
After increasing both the stack and heap, the hard fault still persists.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2019-05-14 12:37 PM
Ah, the fault in USB_WritePacket.
This is simply because of unaligned 32-bit access. Already reported here earlier.
Try to change this way :
HAL_StatusTypeDef USB_WritePacket(USB_OTG_GlobalTypeDef *USBx, uint8_t *src, uint8_t ch_ep_num, uint16_t len, uint8_t dma)
{
uint32_t USBx_BASE = (uint32_t)USBx;
uint32_t *pSrc = (uint32_t *)src;
uint32_t count32b, i;
if (dma == 0U)
{
count32b = ((uint32_t)len + 3U) / 4U;
for (i = 0U; i < count32b; i++)
{
if (((uint32_t)pSrc & 0x3) == 0) {
USBx_DFIFO((uint32_t)ch_ep_num) = *((__packed uint32_t *)pSrc);
} else { //<<< UNALIGNED
uint32_t v;
memcpy(&v,pSrc,4);
USBx_DFIFO((uint32_t)ch_ep_num) = v;
}
pSrc++;
}
}
return HAL_OK;
}
(fast and dirty fix, not optimized, sorry)
-- pa
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2019-05-14 2:37 PM
Thanks for info, I was going to try that next. I've looked for more details on the unaligned memory access, but only found a couple posts mentioning this:
https://community.st.com/s/question/0D50X00009XkgYUSAZ/stm32l4-usb-otg-host-driver-for-cdcncm
The latest STM32L4 firmware doesn't contain USB_WritePacket with the DMA argument. I see the alternate version of USB_WritePacket with dma is in the F7 firmware.
Do you have any links to the previous error report?
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2019-05-14 3:26 PM
Yes, it is the 2nd your link.
Unfortunately, the software team does not have a bug tracker visible for us, and isn't willing to make commitment for updates.
-- pa
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2020-01-22 4:25 AM
Hi,
I want to add useful info about one more solution.
You can emulate serial port in a system on several different Windows versions and interconnect them virtually. So if you have some problem or may be want alternative software, you can try Serial Port Emulator https://www.virtual-serial-port.org/
And i want to say that it is not free, but you have 14 day fully-functional trial.