2016-01-14 11:59 PM
Hello,
I want to use internal bootloader with stm32f103 mcu. I downloaded and installed dfuse tool. My PC is windows 10 and I also tried with windows 7 result is same.. DP pin is pulled up with 5V.At device maganer It didn't work properly as it seems on the picture. Can anyone help me? The trouble may be about driver or windows10 or hardware or MCU model? #dfuse-windows10