2019-12-27 9:20 AM
Please provide a link to the source code of the DFU stock bootloader for STM 32
2019-12-27 9:35 AM
It is not available, the devices have a loader in ROM/OTP. If you are a customer of merit, discuss with your sales contact or FAE.
I think there are other DFU USB examples for assorted "STM32" in their respective Cube?? repositories. These would run from user flash.
2019-12-27 9:41 AM
Can you advise where to get the source code from open sources so that it is easier to understand?
2019-12-27 12:34 PM
Don't know which "STM32" you have
STM32Cube_FW_H7_V1.2.0\Projects\STM32H743I_EVAL\Applications\USB_Device\DFU_Standalone\readme.txt