cancel
Showing results for 
Search instead for 
Did you mean: 

Custom context in callback handlers

Alexander4
Associate

Hello,

I would like to request a feature to be added to the STM32 HAL.

Would it be possible to be able to add a custom user context when registering peripheral callbacks.

Example:

 

HAL_StatusTypeDef HAL_SPI_RegisterCallback(SPI_HandleTypeDef *hspi, HAL_SPI_CallbackIDTypeDef CallbackID, pSPI_CallbackTypeDef pCallback, void* UserContext);

 

And then as callback function:

 

typedef void (*pSPI_CallbackTypeDef)(SPI_HandleTypeDef *hspi, void* UserContext);

 

I really miss this feature and have had to code around it for god knows how many times.

I have added it myself to the SPI driver, but if I regenerate its all gone ofc.

So it would be real nice if this could be added to drivers.

 

Thx,

Alexander

5 REPLIES 5
Pavel A.
Evangelist III

I have added it myself to the SPI driver, but if I regenerate its all gone 

To avoid losing your changes in the HAL libraries:

- When you use Cube to (re)generate code, select the option to create links to the libraries instead of copying all the files into your project. 

- Check your changes in the ST libraries into your version control (yes, make your private branch).

To minimize code differences, do not pass the UserContext as a new argument. Instead, add it to the SPI_HandleTypeDef struct. Then your callbacks will get this arg from the hspi pointer: hspi->UserContext.

 

 


@Pavel A. wrote:

To minimize code differences, do not pass the UserContext as a new argument. Instead, add it to the SPI_HandleTypeDef struct.


@Alexander4 there was some discussion of this in the 2021 thread:

https://community.st.com/t5/stm32-mcus-embedded-software/is-there-a-way-to-provide-context-pointer-to-hal-callback/m-p/182064


@Andrew Neil wrote:

This has been requested before:

Recently (Oct 2024): https://community.st.com/t5/stm32-mcus-embedded-software/feature-request-pass-arbitrary-data-pointer-in-hal-callbacks/m-p/727806

 

Older (May 2021): https://community.st.com/t5/stm32-mcus-products/is-there-a-way-to-provide-context-pointer-to-hal-callback/m-p/182064

 

PS:

Apparently being "tracked internally" by @mƎALLEm:

https://community.st.com/t5/stm32-mcus-embedded-software/feature-request-pass-arbitrary-data-pointer-in-hal-callbacks/m-p/728270/highlight/true#M55730


Escalated as well..

To give better visibility on the answered topics, please click on "Accept as Solution" on the reply which solved your issue or answered your question.

I agree it should have been added to the function argument or to the handler struct.

Alternatively you can create a mapping table.

Some pseudocode:

 

typedef void (*usercallback_t)(SPI_HandleTypeDef *hspi, void* usercontext);

typedef struct
{
  void *peripheral;
  void *usercontext;
  usercallback_t function;
} usercontext_mapping_t;

static usercontext_mapping_t mappingtable[N];

void callback(SPI_HandleTypeDef *hspi)
{
  if (hspi == NULL) return

  for(int i=0;i<N;++i)
  {
    if(mappingtable[i].peripheral == hspi->instance)
    {
      if (mappingtable[i].function != NULL)
      {
        mappingtable[i].function(hspi, mappingtable.usercontext);
      }      
      break;
    }
  }
}

 

 

Create a wrapper function around HAL_SPI_RegisterCallback that automatically registers the function and adds user context to the table. You can also wrap the deregister function.

I prefer creating wrapping functions over rewriting part of the functions. While it adds some overhead in terms of stack and CPU time that usually is not a problem. Once it becomes a problem I would switch from HAL to LL and write my own library.

Kudo posts if you have the same problem and kudo replies if the solution works.
Click "Accept as Solution" if a reply solved your problem. If no solution was posted please answer with your own.