Configure LoRa E22-900M22s module and MAX3485 (for Rs485) into STM32H753ZIT6
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2025-06-18 2:17 AM
Hi, I am working on configuring LoRa (E22-900M22S) and the MAX3485 transceiver to establish RS-485 communication using the STM32H753ZI. I have connected the LoRa and MAX3485 modules as per the following reference:
LoRa(E22-900M22S) | |
LoRa Pin | STM32H753ZI Pin (example) |
MOSI | PA7 (SPI1_MOSI) |
MISO | PA6 (SPI1_MISO) |
SCK | PA5 (SPI1_SCK) |
NSS | PA4 (GPIO) |
RESET | PB0 (GPIO) |
DIO1 | PB1 (EXTI-capable GPIO) |
DIO2 | PB2 (EXTI-capable GPIO) |
BUSY | PB10 (GPIO input) |
GND | GND |
VCC | 3.3V |
RS-485(MAX3485) | |
STM32H753ZI Pin | MAX3485 Pin |
PD8 | DI |
PD9 | RO |
PD12 (or any GPIO with DE support) | DE + RE (tied together) |
3.3V | VCC |
GND | GND |
Could you please guide me on how to configure both LoRa and RS-485 communication using STM32CubeIDE?
- Labels:
-
STM32CubeExpansion (MPU)
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2025-06-18 3:53 AM - edited ‎2025-06-18 3:53 AM
A schematic is a better way to present an electronic circuit.
I'm not clear if you mean that the H7 is connected to the E22 LoRa via RS485, or if these are two separate interfaces?
A complex system designed from scratch never works and cannot be patched up to make it work.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2025-06-18 9:38 PM
Hi @Andrew Neil, in response to your concern, I’ve shared the schematic diagram. Please note that the E22 LoRa and MAX485 (RS485) modules are separate interfaces.
 
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2025-06-19 1:06 AM
You've marked by previous reply as The Solution - but it was really just a question.
Are you saying that you've now resolved the problem?
If not, here are instructions to un-mark it.
@Ematic wrote:the E22 LoRa and MAX485 (RS485) modules are separate interfaces. 
So just handle them separately:
- the E22 LoRa does not depend on the RS485 - it's just the same as any other E22 LoRa application
- the RS485 does not depend on the E22 LoRa - it's just the same as any other RS485 application
Note that the E22 is a third-party product - not ST - so you should go to Ebyte for support with that:
https://www.cdebyte.com/products/E22-900M22S
A complex system designed from scratch never works and cannot be patched up to make it work.