2016-10-09 12:45 AM
I'm getting a basic compile error in stm32f4xx_hal_i2c.c.
The header on the file says: * @file stm32f4xx_hal_i2c.c * @author MCD Application Team * @version V1.5.1 * @date 01-July-2016 I see: HAL_StatusTypeDef HAL_I2C_Mem_Write_DMA(I2C_HandleTypeDef *hi2c, uint16_t DevAddress, uint16_t MemAddress, uint16_t MemAddSize, uint8_t *pData, uint16_t Size) { uint32_t tickstart = 0x00U; /* Init tickstart for timeout management*/ tickstart = HAL_GetTick(); __IO uint32_t count = 0U; The error is: ..\Drivers\STM32F4xx_HAL_Driver\Src\stm32f4xx_hal_i2c.c(2879): error: &sharp268: declaration may not appear after executable statement in block I think we can easy all see the obvious fix to this HAL library file, but I'm struggling to see how anyone could build this (unless they had -cpp flag set) in its released form. Richard P.S. I tried to format this better, but the link that says '''' is no help
#hal-broken2016-10-10 3:41 AM
Hi richard,
Check if the ''C99 mode'' in C/C++ options is enabled.-Hannibal-