2022-07-20 02:12 AM
Hi,
I would ask the community a suggestion for clock configuration.
I should use the USB ans Mass Storage Class using the SD card by SDMMC interface as memory. This function is used for 5 to 10% of my device usage, so I would decrease the SYSCLK for power consumption. Now it is set at 48 MHz.
Which could the right clock configuration to save power? I tried to simply set SYSCLK at 24 MHz but Storage is not recognized any more from Windows. Should I keep SYSCLK at 48 MHz as USB?
2022-12-15 02:08 PM
@Community member I tried this setting:
Using the USB MSC the device is not recognize, while if I use SYSCLK = 48 MHz it is correctly recognized. Which could be a correct clock configuration in order to get a lower clock for power consumption?
Thank you