2011-07-25 8:04 AM
Hi All
As far as I know, the DFU (device firmware update) is specified by the USB org.
I was wondering why ST provides a specific driver for DFU since the DFU class exists and no driver should be required if the descriptors and code are class compliant.
Any idea ?
Maybe the demo project for USB DFU is NOT class compliant ?
I need to provide to my customers a DFU software to allow upgrading the firmware on both Mac & Win, any idea where to find a class compliant DFU source code for Mac ?
Thanks for your answers !
J
#dfu-class-compliant-usb-mac-osx2011-08-08 2:05 AM
ST support, any chance to get an answer ?
Thanks