2018-10-22 4:32 AM
what difference between internal and external phy
Solved! Go to Solution.
2018-10-22 4:52 AM
Hi @nguen nguyen ,
In the STM32F746 MCUs there is two USB 2.0 device/host/OTG controllers:
-> If you want to build your own USB HS application, you have to add an external HS PHY: No on-chip HS PHY embedded in the STM32F746 devices.
Just for your information:
Link to the AN:
Khouloud.
2018-10-22 4:52 AM
Hi @nguen nguyen ,
In the STM32F746 MCUs there is two USB 2.0 device/host/OTG controllers:
-> If you want to build your own USB HS application, you have to add an external HS PHY: No on-chip HS PHY embedded in the STM32F746 devices.
Just for your information:
Link to the AN:
Khouloud.
2018-10-22 7:17 AM
thank so much I think shout use STM32F7x3