Skip to main content
aatif shaikh
Associate III
November 1, 2018
Solved

Can i use Standard peripheral library along with HAL library

  • November 1, 2018
  • 8 replies
  • 1473 views

hello!

as I want to implement TCP/IP and Fatfs based application I have to use HAL library which I'm not very comfortable with. so for other peripherals like USART, SPI and I2C i want to use STD peripheral library which is much easier to understand and implement. or anyone can suggest me an example or reference code using STD peripheral library with TCP/IP stack for stm3220xG eval board.

This topic has been closed for replies.
Best answer by Tesla DeLorean

This is an SDIO+FATFS example for the STM32F4-DISCO with STM32F4DIS-BB, a 2017 refresh of something I put together several years ago.

https://drive.google.com/open?id=0B7OY5pub_GfINVZnNXFvTGxaWmM

This is a damaged thread from one of the prior discussions

https://community.st.com/s/question/0D50X00009XkdmcSAB/stm32f4disbb-fatfs

8 replies

Jeroen3
Senior
November 1, 2018

I have tried. But they are not compatible. Can't even make it to compile.

They both try to define the same things, or different things in the same files. It's a mess.

Tesla DeLorean
Guru
November 1, 2018

Should be example for that board doing LwIP+Ethernet in SPL

https://www.st.com/en/embedded-software/stsw-stm32059.html

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
aatif shaikh
Associate III
November 2, 2018

thanks! it works perfectly fine..

do you know any link where I get some sample code related to Fatfs which uses STD library. cause all I'm getting HAL and STM32CubeMX examples. If available it will be a big help, if not! then I'll have to merge STD and HAL.

Tesla DeLorean
Guru
November 2, 2018

Should be SDIO examples in the SPL trees. Seem to recall some FATFS examples for the EVAL boards. I know I've posted numerous working FATFS examples over the years for F4 boards, the F2 and F4 designso are very similar. ​

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
Tesla DeLorean
Guru
November 2, 2018

STM32F4xx_DSP_StdPeriph_Lib_V1.8.0\Utilities\STM32_EVAL\STM3240_41_G_EVAL\stm324xg_eval_sdio_sd.c

STM32F4xx_DSP_StdPeriph_Lib_V1.8.0\Project\STM32F4xx_StdPeriph_Examples\SDIO\SDIO_uSDCard

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
aatif shaikh
Associate III
November 3, 2018

the example code is very similar to STM32F2xx standard peripherals example of SDIO but I'm unable to find Fatfs example(File input/ output). As I'm not very familiar with SDIO and its working so i don't know how to use other "uSD card" libraries or functions.

Tesla DeLorean
Tesla DeLoreanBest answer
Guru
November 3, 2018

This is an SDIO+FATFS example for the STM32F4-DISCO with STM32F4DIS-BB, a 2017 refresh of something I put together several years ago.

https://drive.google.com/open?id=0B7OY5pub_GfINVZnNXFvTGxaWmM

This is a damaged thread from one of the prior discussions

https://community.st.com/s/question/0D50X00009XkdmcSAB/stm32f4disbb-fatfs

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..