cancel
Showing results for 
Search instead for 
Did you mean: 

bug in HAL library stm32l1xx_hal_gpio_ex.h

dan2
Associate II
Posted on February 23, 2015 at 18:20

The following macro generated by STM32CubeMX 4.5.0 and 4.6.0 is wrong for SYSCFG_EXTICR1-4 when trying to use registers GPIOF, GPIOG, GPIOH for EXTI.

 

&sharpdefine GET_GPIO_INDEX(__GPIOx__) (((__GPIOx__) == (GPIOA))? 0U :\

                                   ((__GPIOx__) == (GPIOB))? 1U :\

                                   ((__GPIOx__) == (GPIOC))? 2U :\

                                   ((__GPIOx__) == (GPIOD))? 3U :\

                                   ((__GPIOx__) == (GPIOE))? 4U :\

                                   ((__GPIOx__) == (GPIOF))? 5U :\

                                   ((__GPIOx__) == (GPIOG))? 6U :\

                                   ((__GPIOx__) == (GPIOH))? 7U : 8U)

Please refer to RM0038 ref manual (DocID15965 Rev 10) pages 216-219.

For SYSCFG_EXTICR1 PF,PG,PH indexes are out of order.

For SYSCFG_EXTICR2-4 Index 5U does not exist.

This issue is related to category 3,4 and 5 devices.

Spent whole day working out what is wrong with my trivial EXTI code using pin13 on GPIOG (STM32L152ZD) :(

Dan

#hal-library #gpio #gpiog
This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
Nesrine M_O
Lead II
Posted on September 07, 2015 at 16:55

Hi,

Please refer to this [DEAD LINK /public/STe2ecommunities/mcu/Lists/cortex_mx_stm32/Flat.aspx?RootFolder=/public/STe2ecommunities/mcu/Lists/cortex_mx_stm32/HAL%20gpio%20libary%20code%20bug&currentviews=53]thread

-Syrine –