2019-12-10 10:06 PM
Dear friends,
I am facing one issue with FOTA on Azure platform.We are trying with evaluation kit (B-L475-IOT01A2)The errors seen are
Download FOTA from: HostName=[stm32blob.blob.core.windows.net] Type=[Secure] port=[443] File=[/firmware-nucleo/Azure_Sns_DM.bin]
Ok reported State [3]: Downloading
-->DeviceTwin CallBack [3]: Status_code = 204
Ok io_interface_description
Ok xio_create
Ok xio_setoption
13-11-2019 15:55:58.183 [RX] - ***\en.fp-cld-azure1\STM32CubeFunctionPack_AZURE1_V3.3.2\Middlewares\Third_Parties\mbedTLS\library\ssl_tls.c (3518): bad message length
***\en.fp-cld-azure1\STM32CubeFunctionPack_AZURE1_V3.3.2\Middlewares\Third_Parties\mbedTLS\library\ssl_tls.c (3729): mbedtls_ssl_read_record_layer() returned -29184 (-0x7200)
***\en.fp-cld-azure1\STM32CubeFunctionPack_AZURE1_V3.3.2\Middlewares\Third_Parties\mbedTLS\library\ssl_cli.c (1454): mbedtls_ssl_read_record() returned -29184 (-0x7200)
onOpenCompleteFOTA
Ok xio_open
Err: xio_send
Kindly help me resolve this issue.
Thanks,
Raju