2013-11-11 02:35 AM
Hi,
I am making a SDR and implementing FM demodulation over it. We chose STM32F4 controllers for our applications yet we are successful in receiving the signal till the DAC's output.
Yet I am still required to make this board more fruitful to us by introducing like a USB
Microphone
device. It just transmits the data to the host as an audio device just like amicrophone
do. Please help me in making my project complete. I am using KEIL uVision for ARM.Continuous Data -> DMA -> USB Buffer -> USB Audio Class -> Detected as USB
Microphone
on PC. #usb-audio-class #stm32f4-discovery-microphone #stm32f42013-11-12 12:15 AM
Hi,
Are you facing any issue with a code you are already using? Or you need an example? Did you checked the examples provided within the USB library (Ex: STM32_USB-Host-Device_Lib_V2.1.0\Project\USB_Device_Examples\AUDIO)? -Mayla-To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2013-11-12 03:22 AM
I have seen this example, this example is for USB Speaker and I need USB Mic
Also, I am unable to run this example on STMF4Discovery.Please help me in running this example.2014-04-28 11:49 AM
Did you find working example for mic input?
2016-03-18 01:48 AM
Hi Mayla,
Would you please help to provide any examples about usb microphone? Thanks a lot! Spencer2016-03-21 01:04 AM
Type in google:
USB �?¼�?¸�?ºÑ€�?¾Ñ„�?¾�?½ �?½�?° �?±�?°�?·�?µ STM32F4-DISCOVERY