Are I2C_START and I2C_STOP commands included in HAL_I2C_Master_Transmit and HAL_I2C_Master_Receive commands?
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2019-08-02 9:37 AM
I am using ​HAL_I2C_Master_Transmit and HAL_I2C_Master_Receive commands to read device ID of various sensors. I wrote a simple code to do that. It works for some sensors (e.g. MCP9800, HDC1080). But it doesn't work for some other sensors (e.g MLX90164, MAX30101, MLX90632, AFE4404). Some of these sensors ask for specific I2C_START and I2C_STOP commands. Following is my sample code for MCP9800;
-----------------------------------------------------------------------------------------------------------------------
buffer[0]=0xFE; //Pointer buffer for Manufacturer ID
HAL_I2C_Master_Transmit
(&hi2c1,0x40<<1,buffer,1,100);
HAL_Delay(500);
HAL_I2C_Master_Receive
(&hi2c1,0x40<<1,buffer,2,100);
IDNumber = buffer[0]<<8 | buffer[1]; //combine 2 8-bit into 1 16bit
UU_PutString(USART2, "\r\nManufacturer ID in Decimal for HDC1080 = ");
UU_PutNumber(USART2, IDNumber);
HAL_Delay(500);
--------------------------------------------------------------------------------------------------------------------
What are HAL commands for I2C_START and I2C_STOP? I couldn't find in the HAL manual.
Thanks
Kiran
- Labels:
-
I2C
-
STM32Cube MCU Packages
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2019-08-04 1:15 AM
Are you sure you should use HAL_I2C_Master_Transmit not HAL_I2C_Mem_Read?
If you're reading data from the sensor's memory then you need to use HAL_I2C_Mem_Read
Tell me if that works
If that's not it, some sensors require a re-start before generating a stop
I didn't find a HAL function that does that in Polling mode
So, you'll have to modify the HAL function to NOT generate a stop
Tell me if this helps
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2019-08-06 2:27 PM
​Hi Ahmed,
Thanks for trying. This didn't help much. But following link helped a lot.
https://community.st.com/s/question/0D50X00009XkXY9SAN/i2c-cannot-read-from-sensor
Thanks
Kiran