cancel
Showing results for 
Search instead for 
Did you mean: 

I would like to know for USB device driver why there is a need for INF file(VID & PID info) and digitally signed cat files with this CMSIS Middleware based USB drivers and why these are not needed for stm32cubemx GUI based USB hal drivers.

GKasi
Associate

I have the following couple of questions

QUESTION :1) what is the difference between USB drivers in the cubemx standard hal library middleware and CMSIS USB Middleware based on the following 2 cases?

CASE:1)  In STM32CUBEMX, When I use STM32 standard Hal library for USB device (through generate code option) , I get USB driver enumerated properly. Send and receive characters works fine with USB serial device com port terminal.   

CASE:2) But If I use CMSIS Middleware USB Device and CMSIS FreeRTOS, the enumeration is happening with Inverted or unresolved yellow symbol as shown in attached pictures in USB Serial Device(COM7) in device manager(Other than thread API code is same as USB Device Virtual Com Port example code provided by arm keil). Does CMSIS Middleware USB device requires any host drivers?

QUESTION:2) I checked in the USB Device Virtual Com Port example code provided by arm keil which uses CMSIS USB Middleware abd CMSIS RTOS from the link http://www.keil.com/pack/doc/mw/USB/html/dev_cdc_tutorial.html and in their example source folder, I could find the following 3 files.

  1. Mcbstm32e-vcom.inf
  2. Mcbstm32e-vcom_amd64.cat
  3. Mcbstm32e-vcom_x86.cat.

I would like to know why there is a need for INF file(VID & PID info) in this CMSIS Middleware and why these are not needed for stm32cubemx GUI based USB hal drivers.

Iam stuck in this for more than a weeks time.

This discussion is locked. Please start a new topic to ask your question.
0 REPLIES 0