‎2025-01-07 11:06 PM - edited ‎2025-01-07 11:09 PM
I am working with the STM32G431 microcontroller and have encountered a discrepancy between the practical and theoretical ADC sampling rates. Here's my setup:
I have toggled a GPIO pin after ADC conversion to observe the sampling rate on an oscilloscope. The measured sampling rate is approximately 142 kHz, while my theoretical calculation suggests it should be around 11.33 MHz.
The theoretical calculation considers the formula:
Sampling Rate=fADC /{ [sampling time(in cycles)] + [resolution (in bits)] +(0.5)}​
Substituting the values:
Sampling Rate=170 MHz / (2.4+12+0.5) ≈ 11.33 MHz
I am unable to identify why there is such a significant difference between the calculated and observed rates. Could it be due to additional overhead, configuration issues, or something else I'm overlooking?
Any insights or suggestions to help resolve this would be greatly appreciated!
Thank you!
‎2025-01-08 12:02 AM
Hi,
1. how you get the idea, the ADC would convert at 11MHz speed ?
Look at ds : absolute max. speed at 12bits is 4 Mhz :
2. The ADC is clocked, so it will convert at the speed you set it - not only theoretical .
Now your measured speed is a bit slow, so you set it very wrong.
3. Read ds + manual , to see how to use it. And dont forget calibration .
Or look at examples from STM , and app.notes ANxxx , to see, how to use it.
‎2025-01-08 12:34 AM
I agree that theoretical calculation may be wrong!.
Now as you the waveforms GPIO in the interrupt is toggling at the 142,8Khz attached image.
System clock is 170Mhz
please help in understanding how I got this 142.8Khz
‎2025-01-08 12:37 AM
please share me the app note links or forum links.
Thanks
‎2025-01-08 12:51 AM
>please help in understanding how I got this 142.8Khz
Well, i cannot know, what you doing...
so at first check, is your system running at xx speed : use MCO pin, set it to main clk /10 , or whatever, and look with a scope on MCO then; just to verify ,your cpu is running that speed, you expect .
Then look at ADC clock: what you set , going to ADC module ?
Then check, whats you do with ADC (read in manual...) , set to the mode (group conversion, single conversion etc.);
and the sampling time you set (dont use 2.5 , except your source is very low impedance; set 6.5 or 12.5 ).
-> calculate speed from ADC clock (/ divider) (/ sampling_time + 12.5 conversion_time) -> maybe:
-> 30MHz / 25 = 1.2 MHz . check it with your bit toggling.
‎2025-01-08 12:56 AM - edited ‎2025-01-08 2:16 AM
app notes ...see at STM :
ed. ->
https://www.st.com/en/microcontrollers-microprocessors/stm32g431rb.html#documentation
+ for forum links : you can try search function yourself ...
‎2025-01-08 1:01 AM
Hello @krushna_moukthik ,
Ensure that the ADC is properly calibrated, this helps reduce offset, gain errors and can affect the accuracy of the sampling rate.
You can refer to these application notes:
‎2025-01-08 1:28 AM
Hello
I am also facing the same issue in the same board :D , my code looks like
while (1)
{
HAL_ADC_Start_IT(&hadc1);
HAL_GPIO_WritePin(PA9_GPIO_Port, PA9_Pin, GPIO_PIN_SET);
}
void HAL_ADC_ConvCpltCallback(ADC_HandleTypeDef *hadc)
{
HAL_GPIO_WritePin(PA9_GPIO_Port, PA9_Pin, GPIO_PIN_RESET);
adcBuffer = HAL_ADC_GetValue(&hadc1);
}
ADC : 12 bit, single ended, 60Mhz(sychronous), ADC1 - IN1, 2.5 cycles sampling time, Fast channel
theoretically, it should be 250ns, but i am getti ng 2590ns
‎2025-01-08 2:05 AM - edited ‎2025-01-08 2:06 AM
So please open a new thread with your question, not capture others ...
‎2025-01-08 7:03 AM
First, you've missed :
Sampling Rate=fADC /{ [sampling time(in cycles)] + [resolution (in bits)] +(0.5)}​
Substituting the values:
Sampling Rate=(170 MHz /ADC Prescaler: Synchronous Clock Mode Divided by 4)/ (2.4+12+0.5) ≈ 11.33 MHz
Second don't use interrupt , better way to verify sampling is to set array for adc samples and feed pwm with known frequency (confirmed with o-scope) to adc input.