2021-09-16 3:51 AM
Hi,
There are host and slave MCU, both are ST MCU.
Slave MCU does not have wifi/ble for OTA upgrade. I would like to use host MCU to download slave MCU image and then use built-in bootloader to upgrade slave MCU.
I can find the communication protocol document of how to use built-in bootloader.
I would like to ask if ST has released any library of built-in bootloader for host? Or I just need to follow the protocol document to write my own library (host)?
2021-09-16 4:23 AM
> I can find the communication protocol document of how to use built-in bootloader.
The general bootloader info is in AN2606.
Specific documents exist for each protocol. For example for UART:
> I would like to ask if ST has released any library of built-in bootloader for host?
ST doesn't publish a library to interface with the bootloader as far as I know.
2021-09-16 9:10 AM
There used to be a tool called Flash Loader Demonstrator, open source things like stm32flash, and I wrote my own years ago just following the protocol docs.
The Arduino MKR WAN 1300 boards use a Murata LoRa modules using an STM32L072, they push in a firmware update using the UART pins and BOOT0/NRST. The Atmel/Microchip processor has 1 or 2MB of space to facilitate this. There is also a pass-thru example
https://github.com/arduino-libraries/MKRWAN/tree/master/examples/MKRWANFWUpdate_standalone
https://store-usa.arduino.cc/products/arduino-mkr-wan-1300-lora-connectivity
If you don't like the ST protocol, something with better flow control like X-MODEM is an option. ST has posted there own IAP examples using Y-MODEM, and I've seen a couple of radio firmware boot-loaders implement that.