2025-03-13 8:13 AM
I have 2 STM32F407 Discovery boards sending data back and forth to each other using usart2. Usart3 on one is just a monitor so I can see the output on a USB comm port. I'm using DMA on the receive for both and the HAL_UART_RxCpltCallback for both just sends the data back for both boards. I have to have a transmit in one of the tasks before it will work. I have a counter that advances in each callback that spins the 4 LED's so I can see if it's working because it goes too fast to spit it out to the comm port. Is there any way to slow it down? I tried putting a vTaskDelay in one of the callbacks but I don't think you can do that. I'm using STM32CubeIDE and FreeRTOS.I have attached both freertos.c files from the Core/Src/ directory. The lights spin incredibly fast and then slow down and pause once in a while.
Solved! Go to Solution.
2025-03-13 11:27 AM
Set a flag in HAL_UART_RxCpltCallback and check the flag in a task. In the task you can use a delay instead of using the delay in the interrupt. In the same task you can transmit instead of transmitting in the interrupt with blocking transmit.
volatile bool dataRdy = false;
void StartTask03(void const * argument)
{
/* USER CODE BEGIN StartTask03 */
/* Infinite loop */
// 57FF70064983574811332087 id of ST-Link for test_uart3
// 066EFF565257867767140832 id of ST-Link for test_uart2
vTaskDelay(10);
HAL_UART_Receive_DMA (&huart2, &data[0], DATA_SIZE);
for(;;)
{
vTaskDelay(2000);
if(dataRdy)
{
dataRdy = 0;
HAL_UART_Transmit(&huart2, &data[0], DATA_SIZE, 10);
}
}
/* USER CODE END StartTask03 */
}
/* Private application code --------------------------------------------------*/
/* USER CODE BEGIN Application */
void HAL_UART_RxCpltCallback(UART_HandleTypeDef *huart)
{
//HAL_UART_Transmit(&huart3, data, 10, 200);
HAL_UART_Receive_DMA(&huart2, &data[0], DATA_SIZE);
dataRdy = true
//HAL_UART_Transmit(&huart3, &data[0], DATA_SIZE, 1000);
//HAL_UART_Transmit(&huart3, &crlf[0], 2, 10);
//vTaskDelay(1000);
if(++menu_ptr > 3)
menu_ptr = 0;
}
2025-03-13 8:53 AM
looking through stm32f4xx_hal_uart.h I found HAL_UART_DMAPause() and HAL_UART_DMAResume(). I guess I'll try that.
2025-03-13 11:27 AM
Set a flag in HAL_UART_RxCpltCallback and check the flag in a task. In the task you can use a delay instead of using the delay in the interrupt. In the same task you can transmit instead of transmitting in the interrupt with blocking transmit.
volatile bool dataRdy = false;
void StartTask03(void const * argument)
{
/* USER CODE BEGIN StartTask03 */
/* Infinite loop */
// 57FF70064983574811332087 id of ST-Link for test_uart3
// 066EFF565257867767140832 id of ST-Link for test_uart2
vTaskDelay(10);
HAL_UART_Receive_DMA (&huart2, &data[0], DATA_SIZE);
for(;;)
{
vTaskDelay(2000);
if(dataRdy)
{
dataRdy = 0;
HAL_UART_Transmit(&huart2, &data[0], DATA_SIZE, 10);
}
}
/* USER CODE END StartTask03 */
}
/* Private application code --------------------------------------------------*/
/* USER CODE BEGIN Application */
void HAL_UART_RxCpltCallback(UART_HandleTypeDef *huart)
{
//HAL_UART_Transmit(&huart3, data, 10, 200);
HAL_UART_Receive_DMA(&huart2, &data[0], DATA_SIZE);
dataRdy = true
//HAL_UART_Transmit(&huart3, &data[0], DATA_SIZE, 1000);
//HAL_UART_Transmit(&huart3, &crlf[0], 2, 10);
//vTaskDelay(1000);
if(++menu_ptr > 3)
menu_ptr = 0;
}
2025-03-13 11:35 AM
Have you tried lowering the BAUD rate?